STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F105RB and correct way to start from a new user perspective

Hi all!I'm starting a new application concerning the driving of a small stepper motor by means of the L6480 driver, I'm also new with the ST software toolchain, so I kindly ask to be patient if some question may be obvious from some certain point of ...

FF1 by Associate III
  • 775 Views
  • 2 replies
  • 0 kudos

STM32L4+USART+Rx+HAL-------Distortion of received data

Hello Everyone,I am using Nucleo-32 board in my project. I am programming USART to receive 10 character data and then transmit this 10 character data back. Problem that I am observing is that if accidentally 11 character it is suppose to display erro...

Find MCU by supported Debug/Trace facility

Hallo all,where can I find an overview on which trace block like SWV, ETM or ETB is implemented in the different STM32 MCUs?Currently I am looking for one supporting ETB for evaluation purposes.Kind regardsStephan

SHoff by Associate
  • 1330 Views
  • 2 replies
  • 0 kudos

Resolved! UART Oversampling 8 and 16

STM32 experts,I bought 2xNUCLEO-F042K6 for testing purposes. Reference manual says that uart speed at oversampling 16 is 3mbit/s, for oversampling 8 is 6mbit/s.Here is my working configuration. I send 100 bytes data at 3mbit/s and oversampling 16 fro...

John Doe1 by Associate III
  • 6696 Views
  • 1 replies
  • 0 kudos

Do Interrupt Priorities Have To Start At Zero?

I've been fighting a very subtle strange QSPI bug for a while now where data is occasionally spuriously clocked out unexpectedly. Without going into too much detail about that right now, my question is about interrupt priorities. I found what appears...

Question on Floating Point operations

I've heard that floating point operations are very time consuming. However, I've seen that many STM32 include a floating point unit. I'm using a L432KC Nucleo. How does it exactly work? As far as I know, L432KC includes this unit which supports hardw...

xpp07 by Senior
  • 2865 Views
  • 6 replies
  • 0 kudos

I used stm32cubemx to config stm32f407, when it entry stop mode, PA0 is used to wakeup MCU from stop mode, how to config system clk. when it entry into stop mode and leave stop mode

entry into stop mode:  HAL_NVIC_EnableIRQ(EXTI0_IRQn);  HAL_PWR_DisableWakeUpPin(PWR_WAKEUP_PIN1); __HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);  HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN1);  __enable_irq(); HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON, PWR_ST...

hjk by Associate
  • 672 Views
  • 0 replies
  • 0 kudos