2018-06-30 2:44 AM
Hello,
The RM says that CAN1 has 16 bit free running timer, can we use this to Tx CAN message at desired interval ? if possible , how to set the desired time period ? or should is use any timer peripheral for my use case?
I am using STM32F446RE nucleo board
Thanks in advance
#stm32-discovery2018-06-30 5:41 AM
what page in the reference manual are you on ?
I think they are suggesting that you can use one of the 17 timers you have...
I use a periodic worker thread to check if I have TxMsgs waiting and if any TxFIFO is available.