STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problem using UART bootloader

I am trying to program a STM32L151UC chip which is placed on a custom board using the bootloader and STM32CubeProgrammer. The connection sequence goes through a few steps until I get a message saying that the chip is in read out protection mode (whic...

ARege by Associate
  • 777 Views
  • 0 replies
  • 0 kudos

Reading 16 bit word with SPI

I have declared the following variable:uint16_t SPIRx;If I use this line to read SPI data, the compiler doesn't throw warnings:HAL_SPI_Receive(&hspi1, (uint8_t *)&SPIRx, 2, 500);But if I say:HAL_SPI_Receive(&hspi1, (uint16_t *)&SPIRx, 1, 500);It thro...

xpp07 by Senior
  • 1006 Views
  • 1 replies
  • 0 kudos

STM32 - USART - where is the REACK bit?

Posted on January 07, 2017 at 17:46Hi,Using the STMF746 DISCO board... looking at the example for USART6 - in the STM32-provided driver code, the software waits for USART.ISR[REACK] to become set.The documentation shows the TEACK bit (bit 21 of the ...

STM32F4 Discovery cycling on/off

This failure happened suddenly with no apparent cause. The board started cycling on/off at a fairly regular frequency (as shown in the attached video). When this happened, LD1, LD2, and LD7 all cycled on/off (LD7 never turns on in normal operation, a...

RDM responder

Posted on December 14, 2015 at 01:07Hi I'm currently developping a RDM responder :) Did somebody of you already took part of a project with RDM ? If so, can I expect some help with my program ? :)Thank you ! #dmx512 #stm32

SPI clock is not clocking!

Hi everyone, i'm trying to read some data from an accelerator and for this purpose using SPI. I'm using NUCLEO-F401RE board. So after enabling SPI, clock pin goes HIGH as i want (CPOL=1) but when i send data CLK stays as HIGH until i disable SPI, mea...

N ORhan by Associate III
  • 2770 Views
  • 7 replies
  • 0 kudos

How does USB FS DFU work to make firmware updates?

Hello I have two cards, the first is a STM32F746 Discovery and the second is a STM32L475 Discovery.I have to use USB FS to do the firmware updates using the DFU class in USB_Device in CubeMx.I have all tried to update the cards with the DfuSe Demo so...

Hani by Associate II
  • 2932 Views
  • 5 replies
  • 0 kudos