STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Timer-Matlab-codegenration

Dear ST community,I'm using MATLAB Simulink to implement a BLDC-motor control. Therefore I use the Target Support Package-STM32 Adapter (STM32-MAT/TARGET).I have problems with the Timer block of this block set.For a simple test, I designed a control ...

OAlsh by Associate
  • 5608 Views
  • 5 replies
  • 0 kudos

STM32F4 with TDC7200 for ToF measurement

Posted on June 22, 2017 at 07:46Hi,I am using TI's http://www.ti.com/product/TDC7200 with STM32F407. The interface is SPI. I am able to read and write into the http://www.ti.com/product/TDC7200 registers (CONFIG1 and CONFIG2) over SPI without any pr...

0690X00000607SGQAY.png

Do we need to enable and set SVCall, PendSV priorities ?

Hello,In stm32cubemx generated code there is the following routine.void HAL_MspInit(void) { /* USER CODE BEGIN MspInit 0 */   /* USER CODE END MspInit 0 */   __HAL_RCC_SYSCFG_CLK_ENABLE();   HAL_NVIC_SetPriorityGrouping(NVIC_PRIORITYGROUP_4);...

ranran by Senior II
  • 1182 Views
  • 0 replies
  • 0 kudos

USE MCU LIKE PL2303A

Hi everyone!How can i use my MCU STM32F407IG like a PL2303 FTDI. Like basically how can i use my mcu as a usb to uart converter? I already worked with the usb device cdc example and i send data to uart tx everything is fine an working but somehow wha...

arduo by Senior
  • 1887 Views
  • 6 replies
  • 0 kudos