STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Measure time difference between 2 PWM using STM32L4

Hi Guys,I working on a project that require measure time difference between 2 PWM (Refer the picture below) . I was able to measure the PWM frequency using input capture method but not able to measure the time difference, Td between 2 PWM. Kindly nee...

LXian.19 by Associate
  • 1235 Views
  • 2 replies
  • 0 kudos

FOC SDK Private Libraries

I see that some libraries from the SDK (Like the PLL State Observer) are delivered as precompiled objects for each of the supported IDE's. Is it possible to obtain the source code of these libraries in order to use them in our project's IDE? (Since w...

kswarm by Associate II
  • 2879 Views
  • 6 replies
  • 1 kudos

Resolved! Why cant debug the nucleo board

Hi, I am learning how to use Uart and created a simple example project where I sent 'hello world'. i then use RealTerm to view this message. i have generated this project using CubeMX and it works however i flashed the board once and after that i can...

MikeP by Senior
  • 1648 Views
  • 3 replies
  • 0 kudos

STM32F769i board novice question

Hi Community,I try to develop my first test app for the STM32F69i board. I got STM32CubeIDE environment working, generated project with all the default settings for this board. According to STM32F769i docs user LED1 and 2 are hooked up to port J, pin...

TDJ by Lead
  • 669 Views
  • 2 replies
  • 0 kudos

ADC3 on STM303F3xx not working (PB0, PB1).

I have an old project already using PA 0,1,2,3,5,7 and PC 1,2,3 as analogue inputs, all on ADC 1 and 2. Due the nature of the project I read some of them in a interrupt timer, and some on demand,when a UART command kicks in. I had to add 3 more ADC's...

Marius CO by Associate III
  • 737 Views
  • 0 replies
  • 0 kudos

Resolved! Help configuring STM32H7 timer

On the Nucleo-H743ZI board, I'm trying to configure TIM3 with a 10 us period. With the internal clock source at 200MHz, I would expect these parameters to create a 10 us TIM3 interrupt:htim3.Instance = TIM3; htim3.Init.Prescaler = 200; htim3.Init...

edwin8 by Associate II
  • 3621 Views
  • 4 replies
  • 0 kudos

How to use QSPI as Single SPI mode?

I am using STM32F779BI for my custom board. I am using TFT LCD Display connected to QSPI, but I want to use QSPI in single SPI Mode. Like simple SPI ( CLK, MOSI, MISO).How to initialize QSPI in Single SPI Mode?

Resolved! STM32F446 FMC SDRAM and linker script

Dear,For the first time, i use an external SDRAM with the FMC peripheral of the STM32F446.I succeeded to describe a in the linker script to place specific data in this section.BUT this section is present in the output file (.hex) when I build my code...

YDann.7 by Associate III
  • 2998 Views
  • 5 replies
  • 0 kudos