STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Why SDIO needs about 3ms on transferring only 512Bytes

Hello, ST experts​STM32F415RGT6 is used on custom board. Everything looks fine except that SDIO opertions. f_write function is called at an interval about 500ms to write 512Bytes to SD card. SDIO_CLK is 24MHz, 4bit bus wide. I really don't know why t...

Yang Yang by Associate III
  • 1094 Views
  • 1 replies
  • 0 kudos

Resolved! PWM RESOLUTION OF STM32F030F4P6TR

Hello, I am new to the embedded community and was facing a problem figuring out the pwm resolution of the STM32F030F4P6TR microcontroller. I went throught the datasheet and the user manual but did not find any solution to my problem.Thanks,Apurv.

AMara by Associate II
  • 1621 Views
  • 4 replies
  • 0 kudos

STM32F7 maximum speed

Recently, I began to deal with the STM32F7 stone, as the STM32F4 lacked speed. By the result, I realized that if you simply run the same program (calculating digital filters) on F4 and F7 at the maximum core frequency, then the performance does not i...

STM32F407 RTC

I use the RTC of STM32F407 with LSE (32.768 kHz).A battery is connected to VBAT for backup.In the reference manual, the Backup operating voltage is at least 1.65V, but the RTC is actually backed up to about 0.3V.I do not know the reason. Could you te...

tyama.19 by Associate
  • 748 Views
  • 0 replies
  • 0 kudos