STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

In STM32H743zi can HRTIM be used as Time Base generator?

Hi ,I need to toggle a GPIO to create a clock pattern for as much as high frequency as possible , So currently using TIM5 and on overflow callback I toggle the GPIO. The generated clock pulse is around 25 us pulse width, I want to decrease pulse widt...

RSrin by Associate
  • 861 Views
  • 0 replies
  • 0 kudos

Did we discuss STM32 in SO8 yet?

https://www.st.com/content/st_com/en/products/microcontrollers-microprocessors/stm32-32-bit-arm-cortex-mcus/stm32-mainstream-mcus/stm32g0-series/stm32g0x1/stm32g031j6.htmlIt's the same trick as in the STM8s in SO8 - several IO pads bonded together on...

i2c problem

here is the read 16 bytes register codeuint16_t TMP_ReadConfReg(void) { __IO uint16_t RegValue = 0;   /* Enable LM75_I2C acknowledgement if it is already disabled by other function */ I2C_AcknowledgeConfig(LM75_I2C, ENABLE); /*---------------...

Microsecond delay using Timer in stm32l0

I have tried below code for generating the microsecond delay for the stm32l0, but its not working.int myTicks = 0;********//Enabling The timerrRCC->APB1ENR |= RCC_APB1ENR_TIM2EN;      TIM2->PSC = 0;      TIM2->ARR = 72;      TIM2->CR1 |= TIM_CR1_URS;...

Writing and reading from Flash on STM32F446

I have a Nucleo-64 Dev Board where I'm developing and testing my automation solution.I'm using the latest STM32CubeIDE and updated STM32 FW Package (1.24.1), FreeRTOS and FATFS as Middleware.I'm trying to wrap HAL Flash Write function, aside a simple...

peppea82 by Associate II
  • 1252 Views
  • 0 replies
  • 0 kudos

Resolved! FMC controller conflict issue

I have 2 FMC controllers on my STM32F429 design. The first controller is SDRAM controller which is used by LTDC&DMA2D as video buffer;The second controller is PSRAM controller which is used as data interface between STM32 and FPGA;​The two controller...

RLee.7 by Associate
  • 1860 Views
  • 2 replies
  • 0 kudos