STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NSS pin has no effect on slave STM32F303 nucleo

Hello,I have two STM32F303RE nucleo boards one acting as a master and the other as a slave.I have flashed the SPI examples on both of them that come with the firmware and both master/slave are working properly.The issue is the example only uses (SCK,...

salman by Associate II
  • 2138 Views
  • 4 replies
  • 0 kudos

Resolved! How many 1.2V internal regulators on-chip for STM32F779NI ?

Hello,Micro-controller used : STM32F779NIQuestion:My understanding is that there are two 1.2 V internal regulators.[1] The regulator that gets enabled by holding BYPASS_REG pin as low[2] The backup regulator that gets enabled through PWR_CSR1.BREAm i...

stm32f103c8t6 conmunication GY-86

Hello evryone.I'm newbie,I need conmunication stm32f103c8t6 and GY-86 with I2C protocol, read data from Gy-86 with debug console in Keil or SW4STM32.I hope someone help me,I try so lost of and I'm fail.Thanks so much!

PThan.15 by Associate
  • 1095 Views
  • 0 replies
  • 0 kudos

Resolved! Generated binary file size in STM32L4

Is there any specific address location in generated binary file so we can know the size of that binary file?Using this, in the firmware to read the size of binary file from that location and use it in our application.

AP_040 by Senior
  • 23450 Views
  • 65 replies
  • 0 kudos

using Labview VISA to control my STM32 Nucleo-F401RE board.

Hello everyone.I wrote a code for my stm32 Nucleo-L432KC board.Now I'm writing code in LabVIEW in order to send instructions (such as: set the User_selection value in the Nucleo board code) and receive data (such as Temperature variable value in the ...

RFink by Associate II
  • 2798 Views
  • 0 replies
  • 0 kudos