STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32L031 noisy, even in reset - EDIT: it's not the STM32

EDIT: it's not the STM32, see latest postHeyho,I have some custom miniature PCBs here, the unholy combination of a super-high-impedance-low-noise amplifier (going to a low noise audio input with 24bit ADC, spectra below from that one) and a STM32L031...

Amp_Noise_MCU_removed.png LCE_0-1742313100646.png LCE_1-1742313120753.png
LCE by Principal II
  • 4195 Views
  • 9 replies
  • 5 kudos

stm32g030 stanby mode current problem

Hello everyone,I have a problem with the STM32G030.My microcontroller is drawing 1.5 mA of current in standby mode. I really can't figure out why. When I put it into stop mode, it draws 25 uA, which is fine, but I can't understand why it's drawing so...

STM32L476 Interleaved ADC Triggering

Hi, I am using STM32L476 Nucleo board to generate and read some signals. I am using TIM3 to trigger TIM1 and generate pwm signals. I also used ADC in interleaved continious mode and everything worked out. What I want to do is that I want the ADC and ...

Stm325_0-1746520119395.png Stm325_1-1746520163296.png Stm325_2-1746520183040.png
Stm325 by Associate III
  • 739 Views
  • 1 replies
  • 0 kudos

HRTIM controlling a PSFB

Hi I have a VERY large driver for a PSFB that unfortunately suffer from a flaw.The idea is that the master timer is reporgrammed with period and CMP1 CMP2 and CMP3 and that the timerD and timerE uses these 4 points for the crossbar. Everything works ...