STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I2C error

MCU:STM32F446RCT6Accessing an I2C device from the MCU may cause an I2C access error.It looks like the last bit of data is missing from the MCU.As a result, access that prevents the device from returning an ACK stops halfway.Attached image "I2C_OK_NG....

syu1 by Associate
  • 852 Views
  • 0 replies
  • 0 kudos

RTC Periodic Wakeup only ocurs once

I am using the STM32L433 RTC in periodic wakeup. i have initialised the rtc and it does interrupt once, but never interrupts again. i suspect the ISR rouitne is not clearing a flag some where. i have seen many comments relating to this but no definit...

FDCAN example on Nucleo H743ZI not working

Hi, So I am trying to use the example of "FDCAN_Classic_Frame_Networking" from the mentioned examples in other thread STM32Cube_FW_H7_V1.2.0\Projects\STM32H743I_EVAL\Examples\FDCAN\FDCAN_Classic_Frame_NetworkingBut I am always caught in an error when...

JFlor.674 by Associate II
  • 1255 Views
  • 1 replies
  • 0 kudos

Resolved! cant reach 64Mhz in STM32G071C8

HiI'm developing on STM32G071C8 with the developing circuitI'm trying to reach 64Mhz as system clockI'm programing RCC->PLLCFGR as follows:R=Q=2 (both on) . P=off N=16 M=2 or N=8 M=1 PLL source=HSI16any combination above 54Mhz - disconnects Flas...

YWhit by Associate III
  • 3266 Views
  • 7 replies
  • 0 kudos

STM32L433 flash update executing from SRAM

Hi,I have a very confusing problem and looking for some outside thinking. I have a project designed around the STM32L433 a nice process that works very well. I am having a problem updating the flash with new firmware remotely. It is an iot type devic...

EMMC support for greater than 2 gb

We are using stm32f769 with 8 gb EMMC , from other forums we understood that there is no HAL support for emmc for more than 2 gb , we are hard coding the emmc block count to 0x773594 and emmc block size to 0x200 . These values are calcuated in accord...

SNNV by Associate II
  • 1783 Views
  • 3 replies
  • 0 kudos