STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

CAN bus on STM32F103RB

Hello, I want to read all message coming from sensor using CAN bus. My configuration seems not okay because the CAN RX interrupt is not trigger. I made the code with CubeMX and below are my files:Main.c#include "main.h"   /* Private includes --------...

NVan.966 by Associate
  • 711 Views
  • 0 replies
  • 0 kudos

Hi I am Using STM 32f407 discovery board. and i coded for the I2C communication some bugs are in the interrupt mode. for receiving one byte

Hi I am Using STM 32f407 discovery board. and i coded for the I2C communication for both blocking and Interrupt API when i using the repeated start condition for receiving one bit in the interrupt condition some bugs are there in the code i don 't kn...

Why I could not receive the data properly in the UART ??

Hi Team, I am using stm32L0 & stm32h7 controller in my design. we can try to communicate from stm32l0(tx) to stm32h7(rx) using UART. stm32h7 While receiving that data was not correct. STML0 was UART Polling mode of transmission. In stm32H7 was Interr...

0690X00000ArpUDQAZ.png
Vel by Associate III
  • 1538 Views
  • 3 replies
  • 0 kudos

Hi, I'm using the MCU STM32l476, and I have a problem with RTC. The RTC works only if the board is turned on. When the board is turned off or it's sent a command to the MCU go to shutdown mode, the RTC is reset to zero values.

According to the datasheet, there is shutdown mode with and without RTC, so I believe it's a problem of configuration. Can be some parameter of configuration that is missing? How to configure the shutdown mode with RTC?Thanks!

FDigi by Associate III
  • 4181 Views
  • 12 replies
  • 0 kudos

I use stm32 eclipse to add two folders in a folder named drivers. One is for my .c files named src and the second is inc for my header files. The .c can not seem to read the header files when called up on.

I use stm32 eclipse to add two folders in a folder named drivers.  One is for my .c files named src and the second is inc for my header files.  The .c can not seem to read the header files when called up on.  I am new to this so the answer should be ...

UART IDLE LINE interrupt

hi, I need some advice, I'm trying to implement the IDLE_LINE interrupt for a UART with DMA. I simply need to receive a variable length buffer. I searched the internet and put together various code snippets, I came to this:in main.c:__HAL_UART_ENABLE...