STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Reading RTC after wakeup from standby mode

Good day,I'm using an STM32L152RE and utilize the standby mode quite often. Upon cold start, I set the RTC and I am able to enter standby mode and wakeup from standby mode based on the RTC time and alarm events.My problem is this: I don't understand ...

Resolved! STM32CubeProgrammer in Linux

Posted on February 22, 2018 at 21:09I have just installed the new STM32CubeProgrammer for Linux but it won't run. I see the error 'Error: Could not find or load main class com.st.app.Main'. Anyone else come across this problem that has a fix?I went ...

Does any one have an example for dual can stm32f407?

Hello. I'm newbie in stm32 family, so I need in high speed bus 500 kbs catch one packet with standart id and change tree bytes. If somebody have an example fow my procesoor dual can, please give it for me. I need trancieve from can1 to can2 all packe...

Resolved! CAN Bus Extid paramater is not transmitting

Hello, I have setup the CAN bus to transmit and has been working fine. I now need a feature which requires the ExtID but this isn't getting transmitted. I have debugged both and can see that the ExtId is getting transmitted but not received, I'm wond...

0690X00000ArnH2QAJ.png 0690X00000ArnGdQAJ.png
MikeP by Senior
  • 3773 Views
  • 8 replies
  • 0 kudos

How are STM32G4 ADC RAIN max datasheet values calculated

The datasheet values for RAIN max are somewhat onerous, as I would need to buffer pretty much all my ADC inputs to support decently fast sampling. But they don't seem to fit with the equation suggested by the design guides. Is there something about t...

0690X00000Aro1jQAB.png 0690X00000Aro2SQAR.png
Lee3 by Associate III
  • 4217 Views
  • 0 replies
  • 0 kudos

Pull up /Pull down of GPIOs in STM32F427VGT6.

Hi,Could you please let me know the default state(Pull up /Pull down) of GPIOs in STM32F427VGT6. Especially I need to know the default state of GPIOs PC4, PB10, PA7 inorder to verify the strapping options for an external Ethernet phy interface. Iam i...

AThom.17 by Associate II
  • 1516 Views
  • 3 replies
  • 0 kudos

Resolved! TIM8_CH2 and TIM8_CH2N at the same time ?

Hello,I am trying to drive a piezo with complementary output from a timer. I am using TIM8_CH2 and TIM8_CH2 as control logic for my piezo command. I expect it to be complementary to increase volume of the piezo. TIM8 is configured as slave of TIM2 th...

SBACO by Associate III
  • 1724 Views
  • 3 replies
  • 0 kudos