STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Where do I read OCxREF?

I need to set up a PWM without an output pin but be able to read the state of the "virtual" signal. In the reference manual this state is referred to as OCxREF (OC1REF, OC2REF etc.). However, I'm clearly going senile as I can't find this in any of th...

PMath.4 by Senior III
  • 1970 Views
  • 3 replies
  • 0 kudos

STM32L151RCT6 PC3 5V Tolerant GPIO

HiIn the STM32L151RCT6 Datasheet (August 2017, DocID022799 Rev 13) it is specified that the PC0 to PC10 GPIO pins are 5V tolerant except the PC3, that should have a standard 3V3 IO structure. We have measured these GPIOs and have found that the PC3 h...

How to use the "errno" in STM32F103CBT6?

Hello!I'm using some of the string conversion functions, who's declarations are present in the "stdint.h" file. at present I'm using "strtol" and "strtod". According to the library "the value of the macro ERANGE is stored in errno, If the correct val...

ULPI clock noise + I/O compensation cell

We are seeing around 400mV of ULPI clock noise (60MHz) on the remaining DAC output with an STM32F427. The data sheet suggests to use the I/O compensation cell when using 100MHz outputs (like all the ULPI interface signals), but information about how ...

stm32f7 uart rx interrupt mode running only once

Hi,we have custom stm32f7 board with debugger connected and we are configuring UART RX in interrupt mode. In main function code is like below and uart rx interrupt is working fine for only once.uint8_t aRxBuffer[15];if(HAL_UART_Receive_IT(&UartHandle...

Tp by Associate II
  • 859 Views
  • 0 replies
  • 0 kudos

STM32F103RCT6 UART5 not working

Hi all,I'm using uart5 of stm32f03rct6 with Std lib but it's not working. However, when i use cubemx with HAL, It works perfectly. Anyone can help me check my code :( USART_InitTypeDef USART_InitStructure; NVIC_InitTypeDef NVIC_InitStructure; GPIO_In...

According to IPC-A-610 revision G, you can have a 30% void in your BGA device. I every pin in the STM32F417IGH6 device was missing 30% of its connection, would the device still work per the datasheet?

IPC-A-610 revision G page 8-93 indicates that you can have a 30% void in your solder ball. We recently had a STM32F417IGH6 device over heat. Upon X-ray, we discovered that about 80% of the solder balls had voids near 30%.