User Activity

Hi,Having our board in which we have interfaced STM32F429 to SRAM (IS61WV204816BLL) .Facing issue while reading back the data after writing.Actual scenario: Have written a SRAM test code in which am writing 10 bytes starting from SRAM location 0x640...
I am using STM32F756 Eval board and trying ADC+DMA example.Example, is about one ADC conversion and the data is stored in variable using DMA.I am looking out for changes to be done in the configuration such that,After I start ADC conversion, I must ...
In a project, want to generate few control signals at a frequency of 5 - 10MHz. with proper synchronization. So i thought of connecting a dedicated crystal at external interrupt pin.Am using STM32F756. Is this controller capable enough to accept the ...
Posted on August 14, 2015 at 11:17Hello,Kindly guide me to resolve this.I have a board having STM32F429 on it. while adding new requirements in the board, a situation has arised such that i am left with no option other than to use port pin PA15 for ...