STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Project/Application with drivers updated

Good morning,I have an application based on the STM32L4 device. When I started working on this application (I use Keil) I used Cube in order to setup the device according to my application. Please, look at attached picture where drivers folder in Kei...

0690X00000BviclQAB.jpg

Building a static library with debug symbols for Cortex-M7

Hi community,We are generating a static library for our Cortex-M7 (STM32H743VI), using the following command:arm-none-eabi-ar rcs libtf.a $(OBJS)How to generate the debug symbols ? (so we can debug the library files while using it in the main applica...

VBrem.1 by Associate
  • 1041 Views
  • 1 replies
  • 0 kudos

Resolved! Get single JSON message sent over Serial.

Hi, This may be an easy thing to answer, but I haven't had much experience. I have a JSON message that I'm sending down to my F446RE board.I am using the HAL_UART_RxCpltCallback function, this works great, however, for this to work I need to know the...

CLH by Associate II
  • 2166 Views
  • 3 replies
  • 0 kudos

Reset generator for stm32

Hi,I have a flash corruption trouble with stm32f103 mcu. While i was reading topics, i have found that a reset generator must be used on system for avoiding flash data corruptions. My device has lots of parameters on stm32 flash, sometimes those data...

er3481 by Senior
  • 2511 Views
  • 6 replies
  • 0 kudos

bldc sinusoidal control

Hi friends,I think my question will repetitive for you guys (in stm-forum) . Actually sorry for that. I have driven a bldc motor with square wave commutation. Which is basically a simple and easy technique. And i have controlled the bldc motor (in s...

Bud by Associate III
  • 1723 Views
  • 1 replies
  • 0 kudos

Doubts about using QSPI for STM32L431?

Now the project uses STM32L431RC external nor flash to save the data. I want to replace STM32L431RB external QSPI flash, which can reduce the cost, but the program byte is too large, so it needs to be put into the QSPI device to run. QSPI flash is di...

STM32L100 TIMx_IC2

Hi there!I have this MCU and i see as an alternate function 14 it can configure PA1 as TIMx_IC2.I cannot find in the documentation or block diagrams the meaning of this function? is it like a TIM_Channel? or like TIMx_ETR?Thanks!

LRold.1 by Associate
  • 849 Views
  • 1 replies
  • 0 kudos