STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hey guys, im new to st and im having hard time with receiving data VIA uart. im trying to receive data with unknown length, decided that the best thing for my application would be idle line interrupt.

my problem is that the DMA only writes to the first address of the buffer, means that when i look on the buffer, the last byte of the message is stored in the first place of the array, and the rest of the data is overwritten.what could be the problem...

DSosk.1 by Associate II
  • 1482 Views
  • 4 replies
  • 0 kudos

STM32F103R8T6 no CAN interrupt?

CubeMX ver 5.4 F1 package ver 1.8.0 and CubeMX ver 5.5 F1 package ver 1.8.0 when using CAN pins PA11 and PA12 the receive interrupt does not work. If you make pins PB8 and PB9 everything works. It also works on any pins if you configure loopback mode...

SBybe by Associate II
  • 681 Views
  • 0 replies
  • 0 kudos

LCD1602+pcf8574 (I2C) and STM32F107

Hi all,I have some problem with LCD1602 + pcf8574 (I2C) and STM32F107pcf8574 operate as SLAVE.I setup i2c in CubeMX and used this tutorial ( https://controllerstech.com/i2c-lcd-in-stm32/ ) to operate LCD, but I failed, then I write a I2C bus scanner ...

MHos by Associate
  • 1921 Views
  • 2 replies
  • 0 kudos

Resolved! Where to find - lowest Vcc value for mcu

Hi, Can someone help me find the minimum voltage Vcc of stm32f103c8.​Lo​west voltage that will allow for maximum clocks frequency. And wont interfere with usb (pullups at data line to vcc).And adc.​2.4 V is minimum when using adc. But will it run at ...

oeliks by Senior
  • 1235 Views
  • 3 replies
  • 0 kudos

STM32F0 for new development

Dear ST community,we are planning using stm32f0 as driver for our X-Y control Unit. with please see the attachment.The requirement is to update the application of stm32f0 via SPI.And we would like also to use the parts of the HAL library.Is those two...

0690X00000BvrolQAB.png
MMatv by Associate II
  • 1763 Views
  • 4 replies
  • 0 kudos