STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to defined Data content inside a Lib but not used by the lib and link this data in Flash memory where i want ? See detail description for more informations

Hello,I try to construct a project but i don't achieve to do what i want.My MCU is an STM32G070CB an I use MDK Essential 5.28 (Flex) Version: 5.28.0.0 with Compiler V6.12.I explain my need :In my projet, my memory space is coomposed of a boot part an...

NLE F.1 by Associate II
  • 1288 Views
  • 1 replies
  • 0 kudos

overwritting existing data in the flash memory

Hello,I have never done this so please be patient haha - I need to store around 10 float numbers into the flash memory - I will do this in the last memory sector. The problem that I have is that I can write & read to the flash but if i want to overwr...

retro by Associate III
  • 4386 Views
  • 4 replies
  • 0 kudos

STM32 Secure boot firmware keys

Hi,I am looking to implement a secure boot system into an application. My product will only be updated OTA.I understand that when a firmware is written i need to hash it and create a digest and then sign it and add it to the hex file payload.Along wi...

CEagl.1 by Associate III
  • 1352 Views
  • 1 replies
  • 0 kudos

Internal PU/PD setting on PA8 of STM32G070RB

Hi,Now, we use STM32G070RB.Please let me make clear about internal PU/PD resistor setting on PA8.Although we set internal PU res from GPIOA_PUPDR, measured voltage is near 0V at this port.We found this is because the PD res that is set by SYSCFG_CFGR...

FYUJI.1 by Associate II
  • 6936 Views
  • 10 replies
  • 0 kudos

built in pull up resistor

i'm thinking about interfacing DHT11 or DHT22 (AM2302) https://www.mouser.com/datasheet/2/758/DHT11-Technical-Data-Sheet-Translated-Version-1143054.pdfhttps://www.sparkfun.com/datasheets/Sensors/Temperature/DHT22.pdfa thing i noted about both of them...

andrewg by Associate III
  • 20475 Views
  • 7 replies
  • 0 kudos

Resolved! Review STM32F405RGT6 minimal design

Hi!I am designing a microcontroller (STM32F405RGT6) circuit board with a minimal configuration.Is this a normal circuit that I developed?The microcontroller will be uploaded firmware on USART1.BOOT1 and BOOT0 are connected to jumpers. Please show me ...

PYaro.1 by Associate
  • 2240 Views
  • 1 replies
  • 0 kudos

Resolved! SPI Burst mode - Maybe?

Hello St Forum! Good to be back at it for another little project here. Good to see familiar names.SPI Going to try and match up an STM32l476VG using SPI to a Ethernet widget. Widget says it can use SPI and apparently it (widget) will auto increment a...