cancel
Showing results for 
Search instead for 
Did you mean: 

Reflash target while connected with X-NUCLEO-LPM01A

Ab.1
Associate

Hello,

I have a STM32L432 Nucleo32 and want to analyze its power consumption with the X-NUCLEO-LPM01A.

I've read that there is the need to open connections to the STLink interface of the target.

After that procedure, is there any possibility to reflash the target (preferably while connected to the X-NUCLEO-LPM01A via CN12/CN13)?

The same question regarding Nucleo-64/-144 can also arise later.

Thanks,

Alex

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0