STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPI - SDO long tail

Hello,I am having problems with STM32C8T6 interfacing with TI ADS8317.Long tail at SDO line (first & second image)The seperation time between each byte is always significantly long (not sure if this is a problem) ( second image)Second image is the en...

0693W000006EMfSQAW.jpg 0693W000006EMgpQAG.jpg
YChen.41 by Associate
  • 1140 Views
  • 2 replies
  • 0 kudos

STM32H745 Extenal Flash QSPI

We are using STM32h745XI board with external memory. But the DISCO board has two QSPI flash 64MB each and total of 128MB. Where as in our custom board we used only one chip as 64MB.But in the project file there is no flash algorithm file for 64MB onl...

YSN by Senior
  • 798 Views
  • 1 replies
  • 0 kudos

Hi, I use STM32F746 to build a modbus environment which connected to RS485 bus.I use as DE-RE pin is not a specially defined alternative function pin, so I defined it as output pin.However I am having a problem receiving the packages I send.

USART3TX--PB10RX--PB11DE-RE--PE15 /*Configure GPIO pin : PE15 */ GPIO_InitStruct.Pin = GPIO_PIN_4; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_MEDIUM; HAL_GPIO_Init(GPIOC, &G...

Bilge by Associate III
  • 893 Views
  • 0 replies
  • 0 kudos

How to Enable Analog Audio in STM32F769I Discovery Board ?

I have a Demo application based on the Audio Playback and record example program . This example defaults to using the onboard digital mics.  I need to use the analog mic/CN6 Line in (blue) jack .  I made changes to use the INPUT_DEVICE_ANALOG_MIC. T...

PR.6 by Associate II
  • 869 Views
  • 0 replies
  • 0 kudos

How to store the data at specific memory location in STM32

how to store the data in specific memory location by using Linker script i found this one in tool how to use this one can any one tell me.ENTRY(Reset_Handler)/* Highest address of the user mode stack */_estack = 0x20009000; /* end of "RAM" Ram type m...

MVENN.1 by Associate II
  • 5972 Views
  • 6 replies
  • 0 kudos

Resolved! Is it possible two use a single crystal oscillator to clock two differnt stm MCUs on the same board?

Hello All,I was wondering if it is possible to clock another STM32 MCU (STMF031) using the single existing crystal oscillator that is currently clocking the main MCU (STM32F334). It could really save me space, power, cost and another clocking source ...

ma.alam9 by Associate III
  • 3718 Views
  • 4 replies
  • 0 kudos