cancel
Showing results for 
Search instead for 
Did you mean: 

Why it's not working to use the same program

JKim.171
Associate II

i'm using two boards for develop, at now.

One board is a nucleo-h743zi. and other board is using a STM32H743IIK processor.

It is the same program, and I wonder why it does not work on the Nucleo-board and on the STM32H743IIK board under development.

Nucleo-board can be debugged using openocd, and STM32H743IIK can be error when using openocd.

I wonder what caused it.

This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6
prain
Senior III

Did you notice the part number difference? 743ZI vs II? they have different package and maybe different register addresses.

JKim.171
Associate II

Hi. prain. thanks' for yours reply answer.

Yes, thay are different packages.

STM32F743ZIT6U ( LQFP 144 )

STM32H743IIK​ (UFBGA176+25  )

I read the data sheets, but the addresses were all the same.

There are only differences in interface support types.

develop enviroment:

OS : UBUNTU 16.04

compiler : arm-none-eabi-7-2017​

​Board Clock : 240MHz ( both are supported up to 480MHz. )

​​

JKim.171
Associate II

STM32F743ZIT6U ( LQFP 144 ) : External Clock 8Mhz ( HSE)

STM32H743IIK​ (UFBGA176+25 ) : External 16MHz (HSE)

TDK
Super User

> Nucleo-board can be debugged using openocd, and STM32H743IIK can be error when using openocd.

Is there a typo here? What isn't working exactly? What is the exact error message you're getting? Can you program okay and only debugging doesn't work?

If you feel a post has answered your question, please click "Accept as Solution".
JKim.171
Associate II

Hi. TDK

OpenOCD Log.

Licensed under GNU GPL v2

For bug reports, read

http://openocd.org/doc/doxygen/bugs.html

Info : The selected transport took over low-level target control. The results might differ compared to plain JTAG/SWD

adapter speed: 1800 kHz

adapter_nsrst_delay: 10000

srst_only separate srst_nogate srst_open_drain connect_deassert_srst

srst_only separate srst_nogate srst_open_drain connect_deassert_srst

Started by GNU MCU Eclipse

Info : Listening on port 6666 for tcl connections

Info : Listening on port 4444 for telnet connections

Info : clock speed 1800 kHz

Info : STLINK V2J33M25 (API v2) VID:PID 0483:374B

Info : Target voltage: 3.242216

Info : stm32h7x.cpu: hardware has 8 breakpoints, 4 watchpoints

Info : Listening on port 3333 for gdb connections

Info : accepting 'gdb' connection on tcp/3333

target halted due to debug-request, current mode: Thread

xPSR: 0x01000000 pc: 0x0800049a msp: 0x2001fff8

Info : Device: STM32H7xx 2M

Info : flash size probed value 2048

Info : STM32H flash has dual banks. Bank (0) size is 1024kb, base address is 0x8000000

Info : Device: STM32H7xx 2M

Info : flash size probed value 2048

Info : STM32H flash has dual banks. Bank (1) size is 1024kb, base address is 0x8100000

target halted due to debug-request, current mode: Thread

xPSR: 0x01000000 pc: 0x0800139c msp: 0x20020000

adapter speed: 4000 kHz

semihosting is enabled

target halted due to debug-request, current mode: Thread

xPSR: 0x01000000 pc: 0x0800139c msp: 0x20020000, semihosting

adapter speed: 4000 kHz

Error: flash write algorithm aborted by target <================================

Info : error executing stm32h7x flash write algorithm<================================

Error: flash write failed, FLASH_SR = 00050000

Error: error writing to flash at address 0x08000000 at offset 0x00000000

target halted due to debug-request, current mode: Thread

xPSR: 0x01000000 pc: 0xfffffffe msp: 0xfffffffc, semihosting

Info : dropped 'gdb' connection

shutdown command invoked

but. STM32F743ZIT6U is normal and good.

stm32cube generated program is

The programs created by stm32cubemx operate well in both cpu.

Up_arch.h

# define getreg32(a)     (*( volatile uint32_t *)(a))

# define putreg32(v,a)    (*( volatile uint32_t *)(a) = (v))

....

putreg32(0XXXXX, STM32_RCC_CFGR);

 ....

​​putreg32 function call and exception genetated.

This is the first time I've ever seen it, so I don't know what caused it.

Don't know

Try with STM32 Cube Programmer

Check if new part is V-step part (ie 480 MHz capable one), might need different SMPS/LDO or VOS settings

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..