STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Wake up from interrupt when use a keypad in polling mode

In my design i have 5 gpio that connecting my keypad , i have 3 row (gpio output ) an 2 col how input , one button keypad is ON/OFF.For me the OFF state corrrespond to sleep state .This is my problem -Before of while i enter i sleep mode :void PW...

bfran.1 by Associate II
  • 3870 Views
  • 5 replies
  • 0 kudos

Resolved! Facing strange issue with STM32G0 RTC

Hello,I am facing a strange issue with STM32G0 RTC. As soon as I initialize RTC, it generates an interrupt and it never comes out of the interrupt. Same program was working previously and suddenly it started throwing this kind of issue. I am wonderin...

0693W000006GMrNQAW.png
HBavi.1 by Associate III
  • 1400 Views
  • 1 replies
  • 0 kudos

STM32 H757 QSPI read not working properly.

Board: STM32 H757Issue: We are using internal QSPI memory. Write is working fine. But reading have issue.reading ignores first byte and also do swapping of 2 byte.For example: --> write 0<offset> 4<number of byte> 1 2 3 4<values to write>--> read 0<...

vro.1 by Associate II
  • 3684 Views
  • 9 replies
  • 0 kudos

Resolved! Problem Running ADC with DMA in single-shot mode

Hello,I'm trying to capture single-shot ADC reading from 3 subsequent channels. I'm using CubeIDE and STM32L100RCT6 on the Discovery board, but I have the same results with STM32F103CBT6. I do everything according to that document, but whenever I try...

0693W000006GABUQA4.bmp 0693W000006G9eqQAC.bmp
Xses by Associate II
  • 1832 Views
  • 2 replies
  • 1 kudos