STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ADC Low power - consumption

Hello,I have a custom PCB with stm32L562 on it. I'm able to put it low power run mode.My consumption is 0.2mA, but if I init ADC the consumption jums to 0.3mA.I've tried to deinit it before going to stop 1 mode but it does not helpHAL_ADC_Stop(&hadc1...

Artuan by Associate II
  • 3963 Views
  • 9 replies
  • 0 kudos

STM32H745 SDIO not working

Hi,I have tested STM32H745 CM7 SD 1bit mode with out RTOS from cube generated files (STM32Cube_FW_H7_V1.7.0) and it's work fine for FATFS file operations, as soon as by adding freeRTOS in cube, the generated files have HAL SD init and f_mount works b...

VDesa.1 by Associate III
  • 1016 Views
  • 1 replies
  • 0 kudos

How to detect IDLE in SMBUS Multi-master?

I'm using SMBus on an STM32F303. The application has the STM32 as host, SMBUS charger and SMBUS battery, the charger and STM32 can act as master.I need to infrequently read from the battery and want to check for IDLE before initiating a transfer.I've...

iguffick2 by Associate III
  • 877 Views
  • 0 replies
  • 0 kudos

Resolved! I2C speed mode is defined only by timing?

When I2C "Speed mode" changes in CubeMX/IDE from Standard to Fast, it seems that only the Init.Timing value changes in generated code.This value goes into TIMINGR register of the I2C .Am I missing anything or this value defines the "speed mode" entir...

Pavel A. by Super User
  • 1610 Views
  • 3 replies
  • 0 kudos

stm32f7 RTC clock waveform is very small

The external RTC clock of stm32f765igt6 chip, the waveform of the clock is very small, RTC clock is very inaccurate. This is whether the crystal oscillator or capacitor selection problem, or our single-chip RTC drive problem; For the external RTC clo...

晓杨.1 by Associate
  • 1237 Views
  • 1 replies
  • 0 kudos

LPTIM CFGR WAVEPOL description

Hello,both STM32L4 and G4 reference describe in LPTIM->CFGRBit 21 WAVPOL: Waveform shape polarity       The WAVEPOL bit controls the output polarity       0: The LPTIM output reflects the compare results between LPTIM_ARR and LPTIM_CMP  registersThis...