STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Preserving SPI data in DMA circular mode

I'm trying to establish communication between a Raspberry Pi and an STM32F407. The Pi is Master and the F407 is a full duplex slave. The SPI is configured with circular mode DMA. When the data is sent from the Pi, I do receive it at the F407. However...

Quectel M66 with STM32L476RG

Hi,Hope everybody is doing great !I am trying to have quectel M66 2G modem running along with our application running on L476RG. I found the celluar package from ST for B96 modem and could integrate it to our application and it has all the features w...

ANaga.2 by Associate II
  • 890 Views
  • 0 replies
  • 0 kudos

STML011 temperature sensor accuracy

Hi,I am having problems measuring accurate temperatures with the internal temperature sensor of the STM32L011D4P7 over the full device temperature range of -40 °C to 130 °C.What I did: Measuring the temperature as described in the Reference Manual (R...

0693W000007BaQ0QAK.png 0693W000007BaQ5QAK.png
Jens_ by Associate II
  • 5552 Views
  • 10 replies
  • 1 kudos

How to implement RFU/OTA to STM32L496?

Hello,So I want to add RFU or OTA to my code as a feature. I saw an rfu source code to one of the expansion of STM32, however it is disabled. I tried to enable it by defining RFU but somehow there are missing files such as se_def.h and se_interface.h...

AMCL by Associate
  • 887 Views
  • 0 replies
  • 0 kudos

unable to debugg Hardfault error on STM32F412ZG

Hello community,I am trying to write time critical code which involves an STM32f412ZG Nucleo 144 board and a RPi communicating over SPI protocol. I have an IMU sensor communicating to STM32 board via I2C interface. I have 3 tasks, which function as ...

0693W000007BZzEQAW.png 0693W000007BZzJQAW.png 0693W000007BZz9QAG.png
AVK.1 by Associate
  • 1499 Views
  • 3 replies
  • 0 kudos

IWDG and CPU Registers

I am working on STM32H7 (Cortex-M7) and using IWDG for monitoring. I am wondering if there is a way to record Cortex-M7 CPU registers (General Purpose (Rx), SP, LR and PC) when IWDG runs out. Either before or after the reset.I understand the RCC regi...

Joyabb by Associate II
  • 1052 Views
  • 1 replies
  • 0 kudos