User Activity

Dear All,I try to use the 2 VCP on the STLinkV3 and I have some problem with standard command...I cannot Send a BREAK command on the TX line I cannot send RST ON/OFF command on the RST line of the VCP2When I use this command nothing append... Any ide...
I try to implement the use of the CubeProgrammer_API.dll in wendev, and it's clearly not design for...1) problem, is struct size, du to alignment... this can be solve using some dummy byte(s)...Main problem not solve at the moment is the call of "rea...
Hello everyone,I try to use CubeProgrammer_API.dll in my oun program and I have a strange thing when I connect to STLink and ask for the list using "getStLinkList"...The answer is correct for the first stlink found but the second one have an offset o...