STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hi all, I'm trying to configure my NUCLEO-H745ZI RAM as Device mass storage, i followed some tutoriels showing how to do this application with CubeMX and Keil IDE but its not working for me. I write my code only in "usbd_storage_if.c" file.

The code compile, load it to flash memory and enter debug mode to run the program.When i connect the usb connector present on the board to test if the computer will detect it as an usb device mass storage, nothing happen ! Can someone help with this ...

PyKe by Associate III
  • 1772 Views
  • 3 replies
  • 1 kudos

Unable to use PC14-OSC32-IN pin in NUCLEO-L152 Board

HI, i am new to STM32 controllers. i am using STM32L151RCT6 MCU in STM cube IDEJust i am trying to use PC14-OSC32_IN pin as input for external IRQ for falling edge configuration ..I not got the proper result , so just i configured that GPIO as input...

MBhir.11 by Associate III
  • 1160 Views
  • 1 replies
  • 0 kudos

Resolved! How to wake MCU from sleep by USART event

I'm learning STM32 by a NUCLEO-L053R8 board.  I want to put device to sleep (not LP Sleep, Stop or Standby) and wake it by either an interrupt or an event.int main() { // Clock and peripherals init // UART init (baud rate, GPIO, etc. are...

p80 by Associate II
  • 1425 Views
  • 1 replies
  • 0 kudos

How to measure the resources (run time / memory consumed) by having part of the code block in external memory encrypted (while using OTFDEC in L5 controller).

I am using STM32L562VE controller. I have configured OTFDEC with a portion of my code encrypted. Is there any way with which I can measure the run time and memory consumed promptly eventhough the code switches back and forth between internal flash an...

VNara.1 by Associate II
  • 829 Views
  • 0 replies
  • 0 kudos

Resolved! M95M02 eeprom Read And Write

Hello All ,I Am working On Interfacing M95M02 EEPROM With STM32 .Anyone Have Example Code for the same that is very helpful for me

Ajeth.11 by Associate III
  • 1838 Views
  • 1 replies
  • 0 kudos

Positive injection on FT pin of unpowered device

Hello, Thanks for the great support . I have a doubt regarding FT pin of the STM32F407x microcontroller . Will the microcontroller gets damaged if 5V is applied when it is unpowered ?in the datasheet Table 12. Current characteristics of section 5.2 ....

n.serina by Associate III
  • 2308 Views
  • 4 replies
  • 1 kudos

Resolved! Timer interrupt flag behavior in encoder mode

I have an STM32G474, but this encoder/timer behavior is likely similar for other MCUs. I have the timer set up in quadrature encoder mode on channels 1 and 2 and I'm using input capture on channel 3. This is tied to the encoder index so that it will ...

Lee3 by Associate III
  • 1966 Views
  • 2 replies
  • 0 kudos

4 digit seven segment display with stm32

Hi,I am trying to interface the 4 digit seven segment display with STM32f3xx by using 74HC595.I am using SPI between uC & 74HC595. If any one having reference for the same then it will be great for me to solve the display switching issue.My data is ...

Bs.1 by Associate II
  • 5701 Views
  • 3 replies
  • 0 kudos