STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Quectel GSM/GPRS AT Command

Anyone Have Example Code of Quectel GSM/GPRS AT Command using UART With STM32 ?If anyone have example code for the same please share with me Thank you in advance

Ajeth.11 by Associate III
  • 3731 Views
  • 2 replies
  • 0 kudos

Resolved! Wrong tick period at 180MHz STM32F446RE

hi everyonei have a strange problem when i try to set clock frequency at high speed.i'm using CubeMX to configure the system and developing on AtollicTrueStudio.i’ve noticed some weird facts setting the clock frequency more than 120MHz.first, is that...

Gzini.6 by Associate II
  • 2975 Views
  • 2 replies
  • 1 kudos

How to reset SPI using HAL functions using Nucleo - L073RZ

I am working on a SPI project (using DMA) as a slave and things seems to work fine but after an hour and maybe more in some cases I see one error and that locks the dma ....I can detect when that happens but I have problems to reset the SPI interface...

JPaz.1 by Associate II
  • 9664 Views
  • 12 replies
  • 0 kudos

QUAD SPI Communication between two STM32H7 boards

Trying to transmit and receive data between two STM32H7 boards using QSPI.As we are new for using QSPI communication,we generated code using STM32CUBEMX and not able to transmit and receive the data.The screenshots for communication between two contr...

Chethan by Associate II
  • 2487 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F469I-DISCO virtual com port USART3?

Hi there,My new STM32F469I-DISCO just arrived I stumbled upon this part in user manual (UM1932):4.11 Virtual COM portThe serial interface USART3 is directly available as a virtual COM port of the PC connectedto the ST-LINK/V2-1 USB connector CN1. The...

PGroe.2 by Associate III
  • 1941 Views
  • 1 replies
  • 0 kudos