STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H7 ADC differential mode, using Vref/2 as INN ?

Hello, Just a quick question as I need confirmation :Using a STM32H7 ADC in a differential input mode, does this circuit work ?  The output of the op-amp is Vout = G * (Vin[+] - Vin[-]) + 1.65 .Then the ADC output should be between :[0 - INT16_MAX] w...

ADesp1_1-1752243111385.png
ADesp.1 by Associate III
  • 1299 Views
  • 4 replies
  • 0 kudos

STM32N6 OTP

Hello,Using the STM32CUBEPROGRAMMER v2.2.0 + the NUCLEO-N657X0-Q :I tried to set the OTP_124 -> HSLV_VDDIO3 bit to 1 but it did not suceed. First, I read the whole otp, put 1 in that field then press Write and it did not work, the OTP_124 stays at de...

FB__1_0-1752207662036.png
FB__1 by Associate III
  • 1468 Views
  • 3 replies
  • 0 kudos

I2C timing on STM32u385 Nucleo

Hi,I am using NCLEO-U385RG-Q  running STM32u385.  I created a project using the board selector.  I configured I2C2 using STM32CubeIDE to run in fastmode at 400khz for PINs PA6/PB2 per schematics described in MB1841.  My clock sources are all defaults...

RiyadAbd by Associate II
  • 2730 Views
  • 5 replies
  • 1 kudos

Resolved! Intermittent failure when entering Standby Mode

Hello,I'm encountering an issue while testing the Standby Mode on my device.Most of the time, the device enters and wakes from Standby Mode successfully. However, after repeated testing, it occasionally fails to enter the mode.What could be the poten...

biopunk101_0-1752200196480.png

STM32Cube MX, VScode setup

Hello.I'm having issues with STM32CubeMX and VScode setup. I have the STM32 VScode extension installed and all the extras that were required as per this page ( https://marketplace.visualstudio.com/items?itemName=bmd.stm32-for-vscode ). I generate a m...

ROVguy by Associate
  • 6044 Views
  • 3 replies
  • 4 kudos