STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to come out from sleep mode using CAN interrupt?

Hello All, I am using sleep mode to save power. I am using STM32L431RC & using CAN interface.I am able to enter into the sleep mode when a CAN message is received. But it doesn't come out when a CAN interrupt is received.My code for CAN interrupt han...

J75888.1 by Associate II
  • 1643 Views
  • 2 replies
  • 0 kudos

Resolved! Why pinrst is configured after sftrst

If you run it with the reset pin, you can use the "__HAL_RCC_GET_FLAG()" functionYou can see that "RCC_FLAG_PINRST" is set.However, when executed with "HAL_NVIC_SystemReset()", "RCC_FLAG_SFTRST" and "RCC_FLAG_PINRST" are set.My expectation is that on...

ckim.2390 by Associate II
  • 2974 Views
  • 3 replies
  • 1 kudos

Help debugging HardFault on STM32F446 using STM32CubeIDE

I have an application running on an ST32F446 using code generated by STM32CubeMX. I use SPI1 in slave mode to receive commands, and have FATFS operating with USB HOST to connect to a USB FLASH drive. I can send commands via the SPI interface to open ...

krubow by Associate II
  • 2380 Views
  • 3 replies
  • 0 kudos

Only single ADC in F401 and F411

This is not a question, more like a statement and proposal to update datasheet.In these two datasheet:DS9716, STM32F401xB STM32F401xC, DS9716 Rev 11, page 105/139DS10314, STM32F411xC STM32F411xE, DocID026289 Rev 7, page 114/149It are specified sample...

Problem with two simmilar projects

Greetings everyone!Lately, I have generated two projects for Nucleo-STM32H745ZI EvB.The first one was generated just for the MCU and for the second one I have chosen the EvB as a reference. So now I do have two quite simmilar projects where the first...

APlot.1 by Associate II
  • 1763 Views
  • 4 replies
  • 0 kudos