STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Where to find systick register documentation for STM32F4 and H7.

Hi,I founded informations about the HAL systick functions, but I found nothing about systick registers in the ref manual of STM32F429/439 and STM32H745/755.For Cortex M3 STM32F10xxx/20xxx/21xxx/L1xxxx, I founded informations in the PM0056 Programming...

o_ by Associate II
  • 3903 Views
  • 2 replies
  • 0 kudos

stm32f303re to write data in the st M95160w EEPROM and reading back the written data. but cannot write accurately. how to do that?

using stm32f303re to write data in the st M95160w EEPROM and reading back the written data. the problem is i am not getting back the accurate output. the output should be like this:status 0x0211 22 33status 0x00but gettingstatus 0x0200 ff ffstatus 0x...

MAlam.2 by Associate II
  • 864 Views
  • 0 replies
  • 0 kudos

16GB eMMC (8-bit) on STM32F676ZI

Hi, I connected a 16GB Sandisk eMMC in 8-bit mode to an STM32F676ZI SDMMC interface.I use HAL drivers and TrueStudio for development.HAL_MMC_GetCardInfo returns this information:CardType : 0 Class : 2293 RelCardAdd : 0 BlockNbr : 2097152...

Jack3 by Senior III
  • 7568 Views
  • 18 replies
  • 1 kudos

Resolved! Low Level API function to register map for STM32G4 family

Hi there,in the ADC FIrmware driver API Description for the STM32G0 family a table exists that shows which LL function accesses what register. In the UM2570 (which is the same doc but for STM32G4) this table is missing. This is giving me a hard time ...

LGard.1 by Associate II
  • 2348 Views
  • 6 replies
  • 0 kudos

I2C LL - no transmit

Got problem after converting from STM32F051 to STM32L051no data transmit.same board, same function:LL_I2C_HandleTransfer(I2C1, 8bitAddress, LL_I2C_ADDRSLAVE_7BIT,1, LL_I2C_MODE_AUTOEND, LL_I2C_GENERATE_START_WRITE);   Timeout=1000000; while(!LL_I...

IIvan.6 by Associate II
  • 1153 Views
  • 0 replies
  • 0 kudos

STM32F427 SPI Enable control

HelloWe select the STM32F427 for new product and use the SPI slave function.​We want to control the SPI enable/disable for the data input control.(SPI_CR1 bit6 SPE) Can the STM32 SPI function receive the data immediately after SPI enabling?​Are there...

TFuji.5 by Associate II
  • 2048 Views
  • 4 replies
  • 0 kudos

STM32H725 4 I2S streams

Hey Guys,I'm struggling to figure out how to stream sine waves at a constant frequency for 8 channels. Each channel has its own sine wave frequency. The issue I'm having is how to stream all these at the same time. I created an array for each sine wa...

0693W00000D02dgQAB.png
KRega.1 by Associate II
  • 4973 Views
  • 10 replies
  • 0 kudos