STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! USART DMA always two times received.

I'm using STM32L476 MCU.I config DMA Setting for USART. And I use HAL_UART_Receive_DMA in main.cIf I received data, test_count always increase two.void DMA1_Channel6_IRQHandler(void){ /* USER CODE BEGIN DMA1_Channel6_IRQn 0 */  test_count ++; /* USER...

0693W00000HpcwSQAR.png
DPaen.2 by Associate II
  • 1757 Views
  • 2 replies
  • 0 kudos

Low Power UART

What is the difference between LPUART and UART?. As far as i read there is no difference to use LPUART and normal one(except power consumption ofc). If I change my UART channel to LPUART, will be any difference? Will be the LP ones DMA usage differ ...

EKosa.1 by Associate III
  • 4494 Views
  • 3 replies
  • 0 kudos

Using Segger Jlink pins as GPIO's

I am developing a project that has M7 processor. I want to use Segger Jlink pin which is JDTI as GPIO.I want to keep it low until I set it. But, while flashing the code to my MCU, JDTI pin becomes high until passing the hal_initialize() function. So ...

EKosa.1 by Associate III
  • 3958 Views
  • 7 replies
  • 0 kudos

Resolved! About the STM32F769I-DISCO board, what are the maximum current consumption and the power input of the external connector ("JP1")?

Hello!I own an STM32F769I-DISCO board which presents an external connector called "JP1" (a picture of this one is given just below) used to power the microcontroller.So, I would like to know:What is the maximum current consumption by this external co...

0693W00000HoQy0QAF.png
LleytoN by Associate II
  • 1666 Views
  • 2 replies
  • 0 kudos

Interrupt based LPUART with BLE application.

Hi I'm working with STM32WB5MMG-dk. The purpose is to develop BLE Gateway. The module has a custom GATT svc with 4 GATT char svc which sends and receive bytes, this data is been provided by MSP430 to STM32WB5 vice versa. So MSP430 acts as master whe...

SPalr.1 by Associate II
  • 6008 Views
  • 7 replies
  • 0 kudos

Resolved! FDCAN - 2 Nucleo G0B1RE Board - What i am doing wrong ?

Hello,I am currently working with 2 Nucleo-G0B1RE board. I adapted the "FDCAN_Com_IT_2_BOARDS" from the G0C1RE-EV example.Clocks are the same, so i think the fdcan is properly setup.I changed the RX/TX pin from PD12/PD13 to PA11/PA12, and connected t...

SBrun.5 by Associate
  • 1211 Views
  • 1 replies
  • 0 kudos