STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H573VIT3Q Programming Issues

We are using the STM32H573VIT3Q in our project and have developed a POC board.While programming via STM32CubeIDE in debug mode, we are encountering random errors (refer to the attached screenshots).Additionally, STM32CubeProgrammer is detecting the c...

Unused pin on STM32F767

Hello.. i m designing a board using STM32F767, could anyone advise what should be done to those unused pins? Ground it or set it to ERC on Altium? 

STM32G071CBT6TR- New Carrier Tape consult

Dear all, Recently, when we were using STM32G071CBT6TR, we discovered some IC bent leads issues. At present, we have not found IC bent leads issues in the original packaging.We are investigating the risk points. Meanwhile, we have also checked the PC...

weihu by Associate
  • 428 Views
  • 1 replies
  • 0 kudos

STM32F407 USB Serial Device class testing

Hey, I have a custom STM32F407 based board with USB.USB_P is connected to PA12USB_N is connected to PA11In the STM32CubeMX I have configured USB Device and in the middleclass I have enabled Communication Device Class (Virtual Port Com) for the Class ...

LPetr1_0-1755067803007.png LPetr1_1-1755067973982.png LPetr1_2-1755068060408.png LPetr1_0-1755069170638.png
LPetr.1 by Senior II
  • 736 Views
  • 2 replies
  • 0 kudos

Error localhost:61234: Connection timed out.

Error in final launch sequence:Failed to execute MI command:target remote localhost:61234Error message from debugger back end:localhost:61234: Connection timed out.Failed to execute MI command:target remote localhost:61234Error message from debugger ...

ADębs.1 by Senior
  • 39748 Views
  • 22 replies
  • 6 kudos

STM32U5 GPDMA cyclic transfer without LLI

Hi all,   in RM0456 is plenty of examples with using LLI but only one without it. And even that contain a block diagram that does not explain anything. Also AN5593 does not mention cyclic transfer. So, here i am. Does this diagram means, that if the...

Eiffel_0-1751715731895.png
Eiffel by Senior
  • 1423 Views
  • 5 replies
  • 1 kudos

Do PWR and SYSCFG need to be clocked permanently?

Hi all: I have a general question about whether STM32 peripherals need to be clocked permanently. I am using an STM32G0 at the moment, and I am disabling the USB C Power Delivery "Dead Battery" feature, in order to make sure that the internal 5k1 pul...

Diez.R. by Associate II
  • 771 Views
  • 1 replies
  • 0 kudos

Resolved! Confirm pin 1 on STM32L433

 I have had a board assembled and want to check they have fitted the STM32 in the correct orientation.  Pin 1 on the PCB is shown by the white triangle. But it’s not clear from the package where pin one is because there are two circles in opposite co...

IMG_3498.jpeg IMG_3497.png