STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Getting wrong value from ADC - STM32G431KBT6

Hi everyone,I'm getting weird values from ADC in a new board that I developed. It looks like it has an offset on it, but a big one.The analog signals arriving in the pins are ok. I tested with a scope. To make sure there was nothing wrong with the an...

SCTimer/PWM equivalent in STM32?

I have a circumstance where two PWM outputs are required, and they must be precisely coupled together. A number of the other big guy's LPC micros included an SCTimer/PWM (that's State Configurable Timer...) which, without too much magic, allows a fi...

DPaul.2 by Associate II
  • 2987 Views
  • 5 replies
  • 0 kudos

STM32H7 Real Time Clock - Sub Seconds

Hi,I need to get time from the RTC at a higher resolution than 1 second. I see there are two reg's that set up the thing for sub seconds, but I don't understand how to use them. I really only need tenths of seconds. I looked at the sub seconds regis...

Debugging STM32H7B3I-EVAL with ETM

Hi,I wanted to debug my STM32H7B3I-EVAL board with J-Trace Pro through ETM interface. According to the manual of STM32H7B3I-EVAL, to enable ETM, R69 must be removed to avoid conflict with the WIFI_SPI4_MISO output, and it's also recommended to remove...

0693W00000JMvdFQAT.png
JSHI.1 by Associate
  • 739 Views
  • 0 replies
  • 0 kudos

Manually include hal library files

Hello! I know that this is not a new topic, and maybe somewhere (even in this forum) someone already answered this question multiple times, but still.....I crawled the forum looking for advice about using the HAL without CUBE, because where I work th...

MFran.4 by Senior
  • 6396 Views
  • 4 replies
  • 0 kudos

How to use BNRG2A1 in low power mode with STM32F401re

I am trying to a develop application that have Temperature sensor and i want to send data to app. but when the device is not connected then i want to put BNRG2A1 in low power mode. what is the way to do that i am using X-CUBE-BLE2 software package in...