User Activity

Hello, I just wanted to ask what's the best way to set the SPI and system clock in STM32L496 to have at least 40MHz frequency for the SPI1. Thank you in advance
Hello, I just wanted to ask if I bought the  NUCLEO-L4R5ZI-P devlopment kit before implementing the STM32L4S5ZI into my PCB. Will it still work with the same code?Thank you Hanya
Hello, I just wanted to ask is there a big difference between STM32L496RE and STM32L4S5ZI. Other than STM32L4S5ZI having a larger RAM and memory. As well as no display interface but with encryption. I'm asking because the STM32L496RE is now out of st...
I have multiple .tflite models that I want to implement in the same project? Is that doable? Also, can I validate data programmatically?Thank you in advanceHanya
Hello, Hope you are staying safe&well. I wanted to ask if I can train the model with new data on the STM32 chip rather on python? Thank you Hanya
Kudos from