STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Communication problem between STM32L432KC to an Ebyte E32.

Hello,I have a project that sends a signal between master (stm32 and Ebyte+antenna) and a slave (another stm32 and Ebyte+antenna) using UART (baudrate 9600) (The communication between the Ebyte and the antenna is fine).My code is fine, it is not comp...

RKavod by Associate II
  • 1484 Views
  • 2 replies
  • 0 kudos

Flash memory problem in STM32H755ZI

Hello everyone, I am having a small project as follows: When I press a button the program jumps to a new program which is located in a new address space. I have successfully tried with STM32F4 series but when switching to STM32H755ZI series which is ...

Resolved! How can I distinguish between STM32F1x medium density devices?

We replaced in our product the STM32F102 MCU with STM32F103 without PCB modification. The 103 contains more RAM and can run at higher frequency and we would like to use the extra resources but there is a criteria. We should use one piece of software ...

NCTUser by Associate III
  • 2612 Views
  • 4 replies
  • 0 kudos

MPU Setup on STM32F4 MCU failed

Dear Forum,I am setting up the MPU of a STM32F401CE using a bare metal system. All tasks and handlers run inPriviledge Mode, therefore I want to enable certain areas for priviledged access, background should cause a memfault. I use the following memo...

LGrüb.1 by Associate III
  • 2464 Views
  • 1 replies
  • 0 kudos