STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Questions about sending RTL8720DN server messages

I made a wifi server with RTL8720DN and connected it to hercules client to send and receive messages, but I can't send them​It worked well to make it a client, send and receive messages from the server,It's a problem sending it to the serverI don't k...

ark2 by Associate III
  • 1056 Views
  • 0 replies
  • 0 kudos

How to find reason for hard fault , very rarely occurring ?

the "system" is a audio player, decoding (in float) MP3 stream, output on I2S to a DAC;cpu H743 , at 200MHz, i/o by DMA1 , stream coming from ESP8266 wlan radio.system ok, running ...maybe 1..3 hours, then hang up:just now got it first time, still in...

0693W00000WHVrDQAX.png 0693W00000WHVsfQAH.png 0693W00000WHW13QAH.png 0693W00000WHW1DQAX.png
AScha.3 by Super User
  • 3759 Views
  • 5 replies
  • 0 kudos

Stop mode in stm32L552

Hi all,I am using stm32L552CE. When I enter stop mode or sleep mode, the current is too high (5mA for stop mode, 18mA for sleep mode). /* Enable PWR clock */  __HAL_RCC_PWR_CLK_ENABLE(); HAL_Delay(5000); printf("Go into stop mode\r\n"); /****** Suspe...

kkid.1 by Associate
  • 1833 Views
  • 3 replies
  • 0 kudos

STM32G071 Push Pull PWM and Fault Pin

Hi,I​ have control H-bridge with 4 IGBTs . PWM Topology : Push Pull Mode PWM Frequency : 10KHz to 100KHzDead Time : 2.5usDuty Cycle : 0% to 50%Emergency Stop : 2 Fault Pins for Individual ChannelsHow to achieve below wave with STM32G071 MCU and STM32...

0693W00000WHUFNQA5.png