STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

[STSPIN32G4]Buck or Gate Dirver EMI?

1. Far-field EMI, as shown in the figure below2. MCU Near-field FFT, as shown in the figure below(EVM also has this situation)3. External power connection, as shown in the figure below4. Use a scope carbon rod and use a ground spring. It is measured ...

0693W00000WJak6QAD.png 0693W00000WJajNQAT.png 0693W00000WJaj3QAD.jpg 0693W00000WJal9QAD.jpg
BChen.11 by Associate
  • 898 Views
  • 1 replies
  • 0 kudos

with Evaluation STM32H7 board, LEDs do not work properly.

In my first stm32 project, I wanted to turn on and off LD1~LD4 on EVAL-STM32H757 board.LD2 and LD4 worked good, but LD1 and LD3 did not work.I set IOC file only RCC and GPIO and Clock Configuration with no error.GPIO Pins : PK3, PK4, PK5, PK6 as GPI...

OhBang by Associate II
  • 2093 Views
  • 5 replies
  • 0 kudos

PC Testing equipment for STM32 boards.

I would like to test STM32F4/L4/H7 based boards with emulated testing software on a PC.I need to test all standard serial communication protocols along with injecting external PPS or interrupt.I need an PCI or USB adaptors or cards, and a software AP...

deckhard by Associate III
  • 1735 Views
  • 3 replies
  • 0 kudos

Resolved! portability between different Cortex-M processors

I have a big project i wrote on stm32F030R8 board, which has M0 processor.However I wat to move the project to another board with M3 processor, Does my code will work ? Or because this is a new board with a diffrent processor, I will need to amendmen...

YShko.1 by Associate II
  • 1355 Views
  • 3 replies
  • 0 kudos

STM32H757XI

Hi! Is there any chance that STM32H757XI will appear at the market with reasonable delivery time? The best result I've found is 48 weeks

Ahov90 by Associate
  • 751 Views
  • 1 replies
  • 0 kudos

Is this the right way to "shut down" a 32F417?

I am implementing a data save procedure when power fail is detected and want to shut down as much stuff as possible to give myself the most time to copy some data into FLASH.Shutting down the CPU has many modes which are quite complicated. I have bee...

PHolt.1 by Senior III
  • 5737 Views
  • 26 replies
  • 0 kudos

Resolved! ADC1 data format? Nucleo-u575 board

Hi everybody! Could please someone enlighten me on the data output format of the ADC1, on regular channels without oversampling, everything is set to default values? Just enabled one channel and converted it. The thing is, I use 2.5v internal referen...

Skfir by Senior
  • 2098 Views
  • 6 replies
  • 0 kudos