cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H723VET6 reference schematic

tzhan.3
Associate

STM32H723VET6: I cannot find the demo board in website? Does it have the demo board?

I need a reference schematic. Can you send it to me?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Peter BENSCH
ST Employee

Welcome, @tzhan.3​, to the community!

What exactly do you want to do with a demo board?

There are currently more than 3400 different STM32 in a wide range of packaging and memory variants, so it makes no economic sense to offer a board for each of them. Instead, there are DISCOVERY, NUCLEO or EVAL boards for selected products, which can be used to start software design while your own hardware is being developed.

In your case (STM32H723 in LQFP100 with 512KB flash) I would recommend to start with the NUCLEO-H723ZG and leave out the pins that are not available later, also only use half of the flash.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.