STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Combine two x- Nucleo boars on the same Nucleo board

Hello, I am new in using the STM32 enviroment,Now I have a project with a x-nucleo- GNSS1A1 and a x-nucleo- IHM08M1 and both projects can run alone on two diffrent Nucleo-F401RE. To safe space an ports at a NUC, they both sending and reseving data fr...

Ten-3 by Associate
  • 791 Views
  • 0 replies
  • 0 kudos

Resolved! General purpose timer

I came across the term in the user manual of L4P5 series that shadow register, auto preload register and auto reload register in timer operationwhat is the difference between three of them?

ajimathew by Associate III
  • 2897 Views
  • 4 replies
  • 3 kudos

How to get the best precision from ADC in stm32f103c8t6?

I am using ADC to read a potentiometer . every time I read 20 data and calculate the average to get a better result. Although the voltage on the ADC pin is stable, the ADC result is not. the final result will be acceptable by reading 100 data each ti...

Zakba.1 by Senior
  • 3076 Views
  • 2 replies
  • 0 kudos

STM32F412ZGJ6TR does not wake up after reset.

my design equipped with STM32F412ZGJ6TR  When applying reset command my STM does not wakeup  We have produced many PCBAs till now without any issue relate to reset mechanism.  The external Hardware reset that was implemented contain Pull-Up resistor ...

Yair S by Associate
  • 2370 Views
  • 1 replies
  • 1 kudos

Resolved! STM32H735 problem

The two buttons next to the STM32H735 I bought fell off during the shipping process. Will this have a great impact on the use?

kuxiang by Associate II
  • 3016 Views
  • 3 replies
  • 1 kudos

STM32G050 DMA problem

I use STM32G050C8T6 DMA for the timer PWM. For the IDE I use STM32CubeIDE. Also in my code block have usart 2 comunication line.Timer PWM work with DMA interrupt. DMA and DMAMUX configuration generated by CubeIDE. When I start the code and if I use t...

ENESK by Associate II
  • 2540 Views
  • 4 replies
  • 0 kudos

Resolved! Production Programming STM32F042 using USB DFU

I am considering STM32F042 in a new product design to provide USB RNDIS interface to the product.Looking at manufacturing options to program the STM32F042 device, I would prefer to use the USB port rather than adding a debug header to the design for ...

HCour.1 by Associate II
  • 3054 Views
  • 2 replies
  • 1 kudos

NVIC

Hi guys. please tell me why you don't do enough NVIC? for example, when several timers are running, and it is necessary to parallelize tasks so that interrupts from each timer happen independently, but now until one interrupt comes out, the other wil...

MTS by Associate II
  • 9492 Views
  • 12 replies
  • 4 kudos

STM32F0xx Bigger size EEPROM emulation AN4061

Hello,I try to adjust the AN4061 EEPROM emulation lib of ST for my STM32F05 controller (1 KB Flash page size) to provide 2 KB data bytes of EEPROM size to use. The reservation of the needed flash pages and the erase page is without problems. The read...