User Activity

Hi, I'm having trouble getting my application to run at a different firmware address.  The end goal is to be able to have the application running, receive new firmware over the UART.  The new firmware will be saved higher in Flash (0x08100000, LENGTH...
I'm using an STM32L4S9 MCU and I'm having trouble getting all the channels to update after starting ​HAL_ADC_Start_DMA. I'm doing a regular 12 bit conversion on 5 channels, trigger by software, waiting for conversion completed in the adc call back ...
320x240 Parallel RGB (LTDC) interface. I've been following the TouchGFX board bring up instructions. I can change the background color, so the hardware side should be good.I made a display in TouchGFX, everything compiles. TouchGFX updated the files ...
I'm setting up a custom board. I was planning to use a NewHaven resistive touch screen with RGB888 and the STM32L4S9. I've been using the stm32F429Disc1 board to learn how to use TouchGFX with Cube IDE. I thought I'd be able to figure out how that wo...
I'm using a STM32F429I-DISC1 board. I can create a display in TouchGFX and it creates the project in the default location "C:\TouchGFXProjects\Display". It makes an IOC file in the "Display" folder "STM32F429I_DISCO_REV_E01.IOC" It makes a "STM32C...
Kudos from