STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB VDD issue

We are using the STM32H7R7L8H6H microcontroller in our product design.During firmware initialization, we observed inconsistent behavior related to the USB voltage detector on different boards that share the same hardware design and firmware.Specifica...

USBVDD.png
Kaushik1 by Associate III
  • 631 Views
  • 5 replies
  • 1 kudos

Resolved! USBPD using CubeMX on H573DK

Hi,I am trying to get USBPD running. I need a simple example code without RTOS. So I used CubeMX. As far as I see it should be easy. All I need to do is:- Turn on the UCPD1 under Connectivity. Here I set "Source". - Turn on the UCPD1 Interrupt- Turn ...

DMA.png Mon.png
RomThi by Associate III
  • 532 Views
  • 4 replies
  • 1 kudos

Help troubleshooting stm32g431 board

Hi. I designed a stm32 board an am trying to program it with a stm32 development board. i am having issues with programming it. This is my board design and my programming setup. I have connected the stm32f4 to my laptop to program it and the Integrat...

WhatsApp Image 2025-10-22 at 16.02.43_99bd9ff3.jpg Screenshot 2025-10-22 161018.png Screenshot 2025-10-22 160147.png aks1_0-1761233999598.png
aks1 by Associate II
  • 3129 Views
  • 26 replies
  • 10 kudos

Programming STM32WB15CCU6E in Arduino IDE

I am trying to program my custom board with STM32WB15CCU6E on it in Arduino IDE. I always upload the code to my nucleo-wb15 board to verify if it is working before uploading it to the custom board. The main difference between the chip used on nucleo-...

mhcheng by Associate
  • 265 Views
  • 1 replies
  • 0 kudos

the external interrupt response time

     Hi,I want to use STM32G431CB or STM32F411CEU6 to measure the time precisely.I need to know the external interrupt response time of GPIO,but I can not find it in datasheet and manual.can you tell me what is the value if the CPU frequency is 100MH...

Huang99 by Associate
  • 424 Views
  • 2 replies
  • 0 kudos

Resolved! STM32U545 : LPBAM cotinuous ADC multichannel

Hi,I am using an STM32U545 on which I expect to use ADC4_IN1 and ADC4_IN18 in stop mode 2 (using LPBAM).I want to create two buffer (buff1 and buff2 uint16_t[32]) dedicated to each input.I want to read 32 samples from input1 then 32 samples from inpu...

Aurelien1 by Associate III
  • 2785 Views
  • 6 replies
  • 1 kudos

STM32G0: PWM Pulse + One-Pulse mode

Above is the configuration of my Timer. - To generate pulse, first I used HAL_TIM_OnePulse_Start but with that pulse was not generate.- So I did this: while(1) { HAL_TIM_PWM_Stop(&htim17, TIM_CHANNEL_1); __HAL_TIM_SET_COUNTER(&htim17, 0); HA...

jowakar122_1-1761976053182.png jowakar122_0-1761976034066.png jowakar122_2-1761976295716.png