STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H750 to STM32WB

I am looking to add bluetooth onto my project. I have an already developed nRF52 project I could use and just connect it through UART to the STM32H750 or migrate my STM32H750 to a WB based MCU since it has onboard bluetooth connectivity. I was wonder...

MAlan.1 by Associate III
  • 2015 Views
  • 2 replies
  • 2 kudos

Build compiler error

I am using STM32U575ZI cortex- M33 controller. I am able to generate a code for the same micro controller in CUBE MX. But in Cube IDE I couldn't able to build the files. It shows some compiler error. like,"../Drivers/CMSIS/Include/cmsis_gcc.h: In fun...

SivM by Associate II
  • 3605 Views
  • 5 replies
  • 1 kudos

STM32H753 How to test ECC on L1 cache

Hello,I am using a STM32H753. I would like to test the ECC on the L1 cache. In my understanding, a double bit error on the data cache would trigger a BusFault: is there a way to produce it? Thank you

lwen by Associate
  • 1181 Views
  • 1 replies
  • 0 kudos

EMW3080 NetxDuo driver for STM32H5

Hi,  I would like to test the EMW3080 with the STM32H5, as I understand it is necessary to load the firmware provided by the ST in order for the EMW3080 to work with the driver provided for the B-U585I-IOT02A board. Correct?Does ST have plans to laun...

AMend.7 by Associate III
  • 2814 Views
  • 2 replies
  • 1 kudos

LWIP

Hey, I am using NUCLEO-H743Z12 and I am trying to configure the ethernet peripheral (and LWIP) with the cubemx with no success (I red lot of manuals online).In the end, I cant even ping my board.Please anyone can help me with the configuration?I main...

Blecher by Associate
  • 1620 Views
  • 2 replies
  • 1 kudos

STM32L552 I2S DMA and CDC continuous transfer problem

I have an ADC connected to my MCU using I2S. MCU configured in I2S master receive mode. MCU supplying the ADC with 12MHZ MCLK. MCU sampling freq is 48 KHZ(Actual is 46.875 KHZ), Number of slots are 4, Data size is 16bits and I2S standard protocol. Us...

Dhanaraj by Associate II
  • 2775 Views
  • 3 replies
  • 0 kudos