STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Missing HRTIM specification for STM32H742/3

Hello,STM32H742/3 datasheet April 2021 DS12110 Rev 8 does not list a HRTIM specifications as e.g. STM32G474 datasheet DS12288 Rev 6 does in section  5.3.16 High-resolution timer (HRTIM). Please provide the data. Best regards 

Resolved! STM32h573 read OTP

Hello,I'm trying to read the OTP flash form my application but I get a hardfault.Is there a read protection or something like that? Here is a code snippet:#define FLASH_START_ADDRESS 0x08FFF000 int main(void) { HAL_Init(); uint32_t* flash_da...

CHeck.1 by Associate II
  • 4135 Views
  • 5 replies
  • 1 kudos

EEPROM in STM32H7 series

Hi, Greetings.Could you kindly confirm whether STM32 H5 and STM32H7 series have inbuilt EEPROM availability?From the datasheets of these series, I could not find EEPROM functionality specifically mentioned.Kindly confirm if there is an efficient alte...

STM32L496ZG MPU test

Hello, I'm trying to implement a MPU test on a STM32L496ZG MCU that will be part of some self-tests in our application. The MPU is working as expected and an interrupt occurs when I try to write to a protected memory region. But now I need to "catch"...

JBiVTSU by Associate
  • 881 Views
  • 0 replies
  • 0 kudos

Resolved! RESET PROBLEMS WITH STM32G474RET6

HelloI am new with using STM MCU's (STM32G474RET6) and encounter very strange reset behavior.In my application reset of the MCU can be done in 3 different ways. 1. Hardware reset - by pressing on button.2. Software reset - by executing NVIC_SystemRes...

error code-38 when starting FD-CAN

Hi,I'm trying to transmit some data using FD-CAN but HAL_FDCAN_Start() function returns error code 38. I have taken reference from STM32H743-EVAL kit example.I have configured same as mentioned there. But still i couldn't figure out the issue behind...

VPras by Associate II
  • 2669 Views
  • 4 replies
  • 0 kudos

Regarding project creation in STM32Cube IDE

This is regarding a new project creation in STM32Cube IDE. I selected STM32U585CITx MCU. After project creation it showed me the following dialog box as shown in the screenshot attached.Please help how to proceed.Screenshot of FirmwareUpdater issue

FirmwareIssue.png
RRR by Associate
  • 1242 Views
  • 1 replies
  • 0 kudos

RTC - CALW bits and calibration PPM calculation

We are using STM32H723 on a custom board.Right now, we are not measuring RTC calibration, we just have a possibility for the user to manually insert values of CALM and CALP elements in RTC_CALR register. We want to inform the user about resulting fre...

heveskar_0-1702302680585.png heveskar_2-1702303622398.png heveskar_0-1702371558418.png heveskar_1-1702302749588.png

Modbus TCP Server-Client communication through Ethernet switch

Hi,I'm using 2 STM32F4 MCUs for Modbus TCP Server/Client implementation based on LWIP. One MCU as a Client and other one as a Server. I have connect both MCUs through D-Link DES-1016D ethernet switch.The problem is when I connect both MCUs directly (...

Screenshot (106).png
Preeti by Associate II
  • 2035 Views
  • 1 replies
  • 0 kudos

USB graceful shutdown before a software reset

I have written a bootloader that is used to update the application code via a Modbus interface over USB.I'm still working on the code to start the bootloader when new firmware is to be uploaded to the custom board.  My board has a buck and an inverti...