STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1554 Views
  • 0 replies
  • 2 kudos

Maximum baudrate error on CubeMX on USART2 STM32F030C8

Posted on June 22, 2018 at 22:03Good afternoon!My name is Alef, I'm trying to set up the usart2 baudRate from STM32F030C8 to 2Mbps but I can not succeed.I'm using 48MHz clock so according to the manual, at 16 samples, I should be able to reach up to...

0690X0000060BpEQAU.png
Alef Rosa by Associate II
  • 2156 Views
  • 4 replies
  • 0 kudos

STM32L4 RTCCLK running slower than HSE frequency

Posted on November 30, 2017 at 05:22Hi All-I'm using SW4STM32 with STM32CubeMx for configuration of an STM32L431RB MCU. I noticed that WakeUp events timed by the RTC appeared slow, and it appears that the RTC is being clocked from LSI rather than LS...

Rea.David by Associate II
  • 2324 Views
  • 3 replies
  • 0 kudos

STM32F042F4 USB cannot be enabled within CubeMX

Posted on June 26, 2018 at 00:49Hi,I'm trying to enable the USB device peripheral for the STM32F042F4 in STM32CubeMX but it is greyed out and I don't seem to be able to enable it. I've checked the datasheet for this part and it seems to support USB ...

0690X0000060BscQAE.png
harris by Associate II
  • 5064 Views
  • 3 replies
  • 0 kudos

STM32CubeMX GPIO setup for RTC calibration clock output

Posted on January 15, 2018 at 13:32Using STM32CubeMX to setup an STM32L496AGIxP controller and configuring the RTC IP to map the calibration clock output to PB2, the initialization procedure of the generated code correctely sets the RTC output remap...

braucadr by Associate
  • 1435 Views
  • 2 replies
  • 0 kudos

STM32CubeMX for STM32H743 USART Interrupt Handling Wrong

Posted on June 19, 2018 at 13:56Information on Wrong Code Creation with STM32CubeMX Version 4.26.0.STM32CubeMX creates wrong call for USART6 Interrupt Handlings for SMT32H743 processor:It generates a call to HAL_UART_IRQHandler instead of HAL_USART_...

GS1 by Senior III
  • 1007 Views
  • 1 replies
  • 0 kudos

Resolved! CubeMX problem

Posted on June 18, 2018 at 10:20hello ST community,I have a little problem with STM32CubeMX.The problem is, when i generate new code with cubeMX to my existing programm, some of my existing work is not working as intended anymore (here it is my I2C ...

CubeMX Project does not generate .elf file

Posted on June 13, 2018 at 15:34Hello,I have just generated a new Project in CubeMX and imported it to Atollic True Studio, but I can't debug it.apparently I am missing a .elf file, and I am not sure how to generate it. Why doesn't CubeMX do this au...

CubeMx erroneous behaviour

Posted on June 15, 2018 at 11:201.  Cube?? version 4.262 . Device STM32F429ZI3. Erroneous module  usbd_conf.c4 Erroneous functions HAL_PCD_MspInit, HAL_PCD_MspDeInit5. CubeMX configuration   see attached conf file.5. Description.when both usb ports ...