STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1599 Views
  • 0 replies
  • 2 kudos

[Issue] CubeMx Assert failed with I2C Low Layer

Posted on April 25, 2018 at 10:17We encountered a problem with CubeMx and I2C Low Layer libraray on an STM32F413RH.The code fall in an assertion.The initialization from CubeMx :  I2C_InitStruct.PeripheralMode = LL_I2C_MODE_I2C;  I2C_InitStruct.Clock...

nicolas b by Associate III
  • 1966 Views
  • 4 replies
  • 0 kudos

BLDC 6 step example and configuration

Posted on July 03, 2018 at 10:15 Hello, I'm using a STM32F303RB on a project. I need to rotate a small and low power BLDC motor. I don't need high speed rotation, I only want to controll it as a stepper and use the 6 step commutation solution in...

0690X0000060LaRQAU.png 0690X0000060LH2QAM.png

Resolved! Issues installing CubeMX on OSX Sierra

Posted on November 23, 2016 at 07:17Hello all, has anyone successfully installed CubeMX 4.17.0 on Mac OSX Sierra (10.12.1)? Every time I doubleclick the install it just bounces and then nothing happens. Any suggestions? #cubemx-macos-sierra

Sam F by Associate II
  • 3399 Views
  • 8 replies
  • 0 kudos

disco/nucleo board ultra low speed ethernet

Posted on June 28, 2018 at 15:04 Hello, im generating default ethernet codes from CubeMX. im using freertos+lwip and i set static ip. All other lwip settings are default. My clock config: My default lwIP settings: My default FreeRtos sett...

0690X0000060LWyQAM.png 0690X0000060LX3QAM.png 0690X0000060LTvQAM.png 0690X0000060LPaQAM.png

MQTT for STM32F0 family

Posted on June 29, 2018 at 15:16Hi,      Please suggest ST microcontroller STM32F051R8T6 can support MQTT protocol.If supports have MQTT library support?Thanks,#stm32cubemx #discovery

CubeMX - UART receive complete interrupt

Posted on June 05, 2015 at 17:08 I'm a little bit confusing with question of UART. So, I need to receive data through UART from PC. Ok, as said in stm32f4xx_hal_uart.c file: *** Interrupt mode IO operation *** =================================== [...

sincoon by Associate III
  • 7836 Views
  • 17 replies
  • 0 kudos

Resolved! STM32CubeMX Error While Downloading Documents

Posted on June 24, 2018 at 09:04STM32CubeMX fails to download documents with the following error:In STM32CubeMX.log (for more details please find attached STM32CubeMX.log:(~~~...2018-06-24 10:50:07,628 [ERROR] ServerAccessManage:989 - Problem during...

0690X0000060BnXQAU.png

CubeMX update to 4.26.

Posted on June 13, 2018 at 09:31Hi, I've updated CubeMX to 4.26. When start a new project, rise many errors for .json files: problem during download (download cancelled). The downloads for packages update work. Any one can help me?#json #cubemx-4.26