cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4 with two SDIO

vinayashree k s
Associate II
Posted on July 26, 2017 at 05:52

I WANT TO KNOW THE STM32F4 SERIES BOARD HAVING TWO SDIO INTERFACES???ANYONE PLEASE SUGGEST ME......

https://community.st.com/community/stm32-community

https://community.st.com/community/stm32-community/stm32-forum

Fahrenkrog.Alberto

simon.scullion

Lappin.Xena

oliverbeirne

sergio.sousa

st.mcu

#discovery #stm32f4 #hal #cubemx #stm32
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Amel NASRI
ST Employee
Posted on July 26, 2017 at 11:48

Hi

vinayashreeks18

‌,

There is no STM32F4 device supporting 2 SDIO interfaces, but you have the STM32F7x and STM32H7x that do (called the ''SDMMC'' instead of ''SDIO'').

To fine tune filter and find the more suitable device for your need, I recommend you to use the MCU Finder tool (either in its own installation or as embedded within the STM32CubeMX). Here an example of what I got:

0690X00000607fzQAA.png

-Amel

PS: Please avoid mentioning space administrators in your post as they cannot provide help in such STM32 specific questions.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

vinayashree k s
Associate II
Posted on July 26, 2017 at 11:52

THANK YOU VERY MUCH FOR THE REPLY

IN STM32F7 SERIES BOARD I GET 2 SDMMC INTERFACES,CAN I USE BOTH INTERFACES SIMULTANEOUSLY???

st.mcu

Posted on July 26, 2017 at 12:11

No limitation on this regard: both interfaces may be used simultaneously.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.