STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1568 Views
  • 0 replies
  • 2 kudos

Why do I miss lib files even with update cubeMX?

Hi everyone,I created this small project.I uploaded package firmware to version 1.11.0 When I generate the code I have all these error messages.The only one we don't need to pay attention is the first error as it's a lib I imported myself.But why I h...

0693W000000X7fvQAC.png 0693W000000X7fqQAC.png 0693W000000X7flQAC.png
psvc.1 by Associate II
  • 2913 Views
  • 4 replies
  • 0 kudos

Partly Disabled Conflict Question from Noob

Sorry for these noob questions, but I am having a hard time understanding the exclamation marks in CubeMX. If somebody could please guide me here, it will be much appreciated.Example 1:The ADC converter is shown as Partially Disabled. However, I shou...

0693W000000WxM5QAK.jpg 0693W000000WxMAQA0.jpg 0693W000000WxMFQA0.jpg
JHenr.2 by Associate
  • 8340 Views
  • 2 replies
  • 3 kudos

UART driver missing in STM32CubeIDE.

I have generated my code using CubeMx tool in STM32CubeIDE. I find the stm32f4xx_hal_uart.c missing from the project. But when I generated the code by enabling the uart as asynchronous mode the second time, the uart appears in the driver folder. Why ...

0693W000000WSkkQAG.png
PKuma.51 by Associate II
  • 1479 Views
  • 2 replies
  • 0 kudos

Bug report: code generation STM32L475 IOT board

When I want to use the X-CUBE-BLE1.5.0.0 on STM32CubeMX, the file "b_l475e_iot01a1_bus.h/c" is not generated. Thus the project cannot be compiled.To reproduce:create new project on B-L475E-IOT01A boardoption of Targeted Language: C++Initialize all pe...

PADAM.1 by Associate III
  • 3669 Views
  • 9 replies
  • 1 kudos

Resolved! NRST stuck in reset_state

Hello,I am assigning pins on a STM32F446 micro in cubemx.I would like to give a pin name to NRST, but it is stuck in a reset_state, and won't let me change it. It is colored differently than other pins.Is it possible to change NRST, or does it stuck ...

0693W000000X8fSQAS.png
JAzri.1 by Associate
  • 1384 Views
  • 1 replies
  • 0 kudos

How do I program my STM32L4R9 with SDMMC and FatFS?

Hello,I would like to write a simple program for writing CSV files to a micro SD card on a custom board I made with my STM32L4R9. The card works on 3.3V and my STM on 1.8V, so I'm using a level shifter.For now, I selected SDMMC1 4 bits wide bus and F...

GMelo.2 by Associate II
  • 2452 Views
  • 5 replies
  • 0 kudos