STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1568 Views
  • 0 replies
  • 2 kudos

STM32F042C4U6 memory too small for cubeMX generated project.

I've used a STM32F042C4U6 in a simple application requiring USB. I'm using cube IDE. When the project is generated with cubeMX and compiled, it is too large to fit in memory before I've even added any user code. Is this right ? If so, what is the poi...

CDamp.1 by Associate
  • 2515 Views
  • 5 replies
  • 0 kudos

Problem loading STM32CubeMX on Mac

Hello,I am trying to install STM32CubeMX IDE on my MAC, and I get the following message:"This package is incompatible with this version of macOS.The package is trying to install content to the system volume. Contact the software manufacturer for assi...

Flyindon by Associate II
  • 4021 Views
  • 5 replies
  • 1 kudos

Why is STM32 CubeMX not running?

HiUntil three days, CubeMX runs nice at my laptop. Now (possibly after java update), CubeMX shows the light blue start screen, and stops without any message.New installation didn't solve the problem, uninstallation fails also.Launching from console f...

OLenz.1 by Associate II
  • 3580 Views
  • 5 replies
  • 0 kudos

CubeMX confusing ADC trigger selection

At register level selecting ADC trigger event is done thru EXTSEL with many internal sources (timers) and one external (EXTI Line 11). Consistent approach is in LL API, where selecting trigger source by "LL_ADC_REG_SetTriggerSource" function or thru ...

0693W000001r522QAA.jpg 0693W000001r527QAA.jpg

Hello everybody, I'm trying to program an STM32F446RCT6. It should run from HSE, which works fine after loading the program on the chip, but after rebooting (switching the voltage source off and on) it does nothing.

I have already tried to use a second SystemClock_Config (copied from a fresh project after code generation), to first use the HSI after reboot and initialize everything (USART, GPIO,...), and then switch to the HSE, but it didn't work.I would appreci...

MBjel.1 by Associate II
  • 2373 Views
  • 5 replies
  • 0 kudos

Migration from SPL to HAL on STM32

I'm migrating an ST driver file from the old standard peripheral library to the new HAL system. Here's and one example of many identifiers I'm having to replace:Old: ETH_DMA_Rx_Frame_infosNew: ETH_DMARxFrameInfosThese two identifiers contain EXACTLY ...

Aasdf.1 by Associate
  • 2552 Views
  • 2 replies
  • 0 kudos

Cube AI and model Keras

Hello,I get an issue when I try to load a Keras model in CubeMX (see image).When I click on Validate on Desktop, all results are 0: acc, rmse and mae. Is it a bug on CubeMx?I have the same result even if I compress my model. And I try another model w...

IFaye.1 by Associate II
  • 2659 Views
  • 3 replies
  • 0 kudos