STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1674 Views
  • 0 replies
  • 2 kudos

How to write a custom package for CubeMX?

Hi, I have written a custom driver for Modbus protocol and I want to share it with others, I think CubeMX is the most convenient way to share it.​I found that CubeMx does use .pdsc files to install packages, and I have written a simple .pdsc file to ...

NGe.1 by Associate II
  • 2061 Views
  • 3 replies
  • 0 kudos

use LAN8720a for PHY (init ethernet)

Posted on September 27, 2016 at 11:50hi I working with stm 32 f 429 with cubemx (to init ethernet)in cubemx PHY is DP83848 but i using LAN8720aWhat changes should be in Keil (FOR Lan8720a) ?any body know?There is contents dispersed in some page in t...

hamrgh by Associate II
  • 10286 Views
  • 11 replies
  • 0 kudos

Ipv6 self-assigned address (Stateless autoconfiguration)

I am using STM32f769Ni discovery board. I need to transfer the data from discovery board to another node via ethernet. Here i have to use the discovery board as client.Another node acting as server. I need to use the Ipv6 self-assigned address(statel...

KP.1132 by Associate II
  • 1377 Views
  • 1 replies
  • 0 kudos

Saving data to SD card

Hello everyone,In CubeMX 5.3.0 I have configured FATFS+DMA+SDMMC for a card running STM32F777VI. i've been trying to save some data into a .txt file.It works fine, but i can't write data to SD card as fast as I want. Requirement is to save 25 bytes ...

0693W000001tTBMQA2.png 0693W000001tTBbQAM.png
HChau.2 by Associate
  • 1676 Views
  • 2 replies
  • 0 kudos

How to import CMSIS DSP library without using CubeMX?

Hello everyone. I'm trying to use some functions available in the CMSIS DSP Library.First I tried to add the library through CubeMX->Additional Software, but found a known bug reported here. According to this link, this bug should be fixed for the ne...

Ajudi.1 by Associate II
  • 2112 Views
  • 3 replies
  • 0 kudos

No updates for CubeMX?

CubeMx has not found any updates. Do they still arrive by autoupdate in Cube or should I search in GitHub?

LMI2 by Lead
  • 865 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.