STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1568 Views
  • 0 replies
  • 2 kudos

Resolved! I can't find the PULL UP menu in STM32CubeMx. (to use i2c1)

Hi AllI have simple question about STM32CubMX.I use the STM32F103RBT and test the i2c with eeprom.When I set the pin for i2c, I should change the GPIO Pull-up/Pull-down in STM32FCubMx.But This menu is not in STM32FCubMX.I don't connect external pull ...

0693W000007ERMPQA4.png
dKim.1 by Associate II
  • 4012 Views
  • 2 replies
  • 0 kudos

Are STM32F7Cube code examples configured with CubeMX ?

Hi, The SDK package provided in STM32F7Cube has many code examples on all topics but is that code initialized with CubeMX ? Or, otherwise , if it is not , in order to reconfigure or customize it the user has to manually merge that code with the one ...

eBirdman by Senior II
  • 1373 Views
  • 2 replies
  • 0 kudos

H7 LL EXTI 1.8.0 fails to enable interrupt, but works with HAL

Using STM32CubeIDE 1.5.1, H7 firmware library 1.8.0, NUCLEO-H743ZI:The blue "User" button is tied to PC13. Using the HAL library, I am able to generate an interrupt when the button is pressed (rising edge).When I change the GPIO to use the LL librar...

dale by Associate III
  • 853 Views
  • 0 replies
  • 0 kudos

Resolved! Why no Synchronous Trace option for STM32G474RE in CubeMX?

Hi,I am trying to set Debug under Sys to "Synch Trace" in latest CubeMX but there is no such option for my STM32G474RE: On other screenshots on the internet I see those options: Any idea why?Is Synch Trace not available on the 64 pin package???Thanks...

0693W000007DtxqQAC.jpg 0693W000007DtyjQAC.jpg
Anguel by Senior
  • 1187 Views
  • 2 replies
  • 2 kudos