cancel
Showing results for 
Search instead for 
Did you mean: 

Installation issue

AXu.11
Associate III

When I install the STM32CubeMX in Windows 10 it prompts requiring Java 1.8.0_45(64-bit), in fact there is Java 1.8.0_261_b12 in my computer and my computer is 64_bit but it can't recognize.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Aymen CHAKROUN
ST Employee

Can you please follow theses steps:

1- Remove you current JRE from Windows

2- Download the JRE 64-bit (Offline installer package), through this link

0693W000003QKcEQAW.jpg

3- Install STM32CubeMX

I'm waiting for your feedback,

Aymen.

View solution in original post

9 REPLIES 9
TDK
Super User

It may be seeing a different Java installation. What is the exact output of "java -version" from the command line?

If you feel a post has answered your question, please click "Accept as Solution".
AXu.11
Associate III

JAVA_VERSION="1.8.0_261"

OS_NAME="Windows"

OS_VERSION="5.1"

OS_ARCH="i586"

SOURCE=" .:148386d4b327 corba:7bba472d7452 deploy:3bc2e14623db hotspot:1a97f34cea08 hotspot/make/closed:e11b6693ad95 hotspot/src/closed:21fdb178e79d install:df9a079c476a jaxp:0741fb08db6d jaxws:62a7981fdbd8 jdk:cd33dd84ca12 jdk/make/closed:c0061afa7a2a jdk/src/closed:9fe66686fb70 langtools:dc513ee0a27c nashorn:be9a82e37fea"

BUILD_TYPE="commercial"

Aymen CHAKROUN
ST Employee

Hi @AXu.1​ ,

According to your "java -version", the installed JRE is 32-bit.

Can you please uninstall the actual JRE and re install new JRE 64-bit?

Regards,

Aymen.

AXu.11
Associate III

Hi! Aymen,

It distinguishes 32/64 bit automatically and the Java works in Edge. Please see appendix.

Regards,

Adam

AXu.11
Associate III

This forum only upload one appendix

AXu.11
Associate III

One more

AXu.11
Associate III

Last one is repeated

Aymen CHAKROUN
ST Employee

Can you please follow theses steps:

1- Remove you current JRE from Windows

2- Download the JRE 64-bit (Offline installer package), through this link

0693W000003QKcEQAW.jpg

3- Install STM32CubeMX

I'm waiting for your feedback,

Aymen.

AXu.11
Associate III

Hi! Aymen,

I've installed ST32CubeMX successfully based on your link. This Java works.

Now www.st.com web site also works regularly.

Thanks for your support.

Regards,

Adam